Other Parts Discussed in Thread: EK-TM4C1294XL , EK-TM4C129EXL , MSP430F6659 Hi all,
I'm having some trouble interfacing with this LCD that I'm working with. The model for the LCD is NHD-5.0-800480TF-ATXL#-CTP, and it uses the controller board NHD…
Hi Board designers
We currently do not support schematics review over E2E.
You could do a self-review following the below steps that includes detailed custom board schematic design guidelines and schematics review checklist.
In case if you have…
Dear experts,
I was hoping you could provide me with some help getting the ASP with EDMA up and running.
Hardware:
I am using the Davinci-DM644x EVM by Spectrum Digital, but only the DSP side. The ASP is connected to external device, which provides…
Part Number: TPS53667 Tool/software: Hi team.
I have several questions regarding PMBus specification. TPS53667 is daisy-chained with PMBus and I2C in my customer's usecase.
1. is it possible to do daisy chain with PMBus and I2C on same bus(data line…
Hi Carrie ,
I ve at the end dumped all UB960 registers so please you can have a look and tell me "yes" or "no" if there should be valid signals in CSI TX port 0 lanes?
fie in attach
thank you
best regards
Carlo single-cam-ar0233-colorbar9.t…
Part Number: BQ78350-R1 Other Parts Discussed in Thread: BQSTUDIO Hi,
I think I did not understand completely the SoC algorithm in the bq78350-r1.
First thing:
1) SoC is completely wrong after a reset of the device. I use a Samsung 50E 21700 cell…
Part Number: BQ40Z50-R3-DEVICE-FW Other Parts Discussed in Thread: BQ40Z50 HI
I am trying to put BQ40Z50 into sleep mode, this is for testing power consumption of the BQ40Z50R3 in sleep mode. I am sending ManufacturerAccess() 0x0011 SLEEP Mode command…
Part Number: BQ40Z50-R3-DEVICE-FW Hi
I am trying to test the fuse pin of the BQ40Z50R3, but when I have sent 1D from BQ Studio I am getting the following errors. I am also attaching the settings for your reference. I would like to understand any settings…