Part Number: CC1310 Hi guys, this happened to at least in 6 boards powered by CR2032 batteries, which drained completely. When removing the battery and measuring the current, there's a constant consumption of 15mA, and the program of the cc1310 microcontroller…
Part Number: AM2732 Other Parts Discussed in Thread: TMDS273EVM Tool/software: Hello i'm working with AM2732 evm board and i need to power it from "Fuse box" of Truck. could you please advice me which circuit can I build it to protect and power my AM2732…
Part Number: LM5012-Q1 Other Parts Discussed in Thread: LM74700-Q1 Tool/software: Hello,
We have used LM5012-Q1 in our design. the input is 24V and we expect 12V at the output but we get 12.55V !! here is the circuit:
I checked the values for…
Part Number: LM5012-Q1 Other Parts Discussed in Thread: LM74700-Q1 , LM5012 Tool/software: Hello,
We have used LM5012-Q1 in our design. the input is 24V and we expect 12V at the output but we get 12.55V !! here is the circuit:
I checked the values…
Part Number: TIDM-SOLAR-DCDC Tool/software: Dear TI Community,
I'm working on a solar-powered system that requires a battery charging circuit, buck-boost conversion, and multiple output voltages. I'm looking for recommendations for suitable TI ICs to…
Part Number: TMS320F280049 Tool/software: Hello,
We would like to know the Switching frequency used by the Internal 1.2V Switching DCDC Converter on the TMS320F28004x DSC.
Regards,
Part Number: LM5158 Other Parts Discussed in Thread: UCC33420 Hi,
I am looking for an isolated DCDC with the following conditions. In the case of isolated on-board power supplies DCDC (manufactured by other companies), the bottlenecks are the height…
Part Number: TPS7H6003-SP I'm looking to build a syncronus dcdc boost converter to go from 12V to 200V based on the topology below. The PWM signals will be generated by a microcontroller running a control loop. This is needed so the output voltage can…
Part Number: INA180 I am utilizing the INA180 for monitoring DCDC current. The INA180 amplifies the voltage across the current sensing resistor, presenting a sine wave pattern as observed on the oscilloscope. Consequently, despite a stable output current…
Part Number: CC2642R-Q1 Tool/software: Hi,
Can the 6.8uH inductor be changed?
background, Customer has the TIS issue when use the 6.8uH inductor. when they tune this to 4.7uH, the TIS is improved significantly.
BR. Albin