Other Parts Discussed in Thread: LM3409,
Hello,
I am using DAC8563 to set the IADJ pin on LED driver LM3409. This is a DC value, it is set once via software and stays the same value. VREF is 1.25V, I'd like to be able to use the full…
Hello! I tested my DAC8563 on a STM32H743 but it doesn't work (0V on A & B Channels)...
So I tried with an Arduino UNO and it's OK.
Times ago I used different STM MCU without problems (F4, F7).
This is STM SPI initialization…
Hi Team,
What are the differences between the DAC8563 and the DAC8563T? Is it just the TTL enabled I/O on the T version or is there other differences?
Thanks,
Matt
I have a new sensor design using the DAC8563 chip. The DAC output signals (VoutA, VoutB) are fine until I begin the RFI/EMC immunity tests.
When the DUT is subjected to an RF power of 10V/meter, the DAC output voltages shift. During…
The data sheet on pages 6 and 7 shows different values for the noise density: 250 nV/√Hz@1KHZ (on page 7) and 90 nV/√Hz (on page 6) What is the difference between these two specs and which is the actual number?