Other Parts Discussed in Thread: TINA-TI,
Tool/software:
Hello,
I need a .lib file of this component for a TINA-Ti simulation.
It could be another operational amplifier that can works at 200ºC.
Thanks in advanced.
Asier
Tool/software:
Hello,
I'm needing a cross for the below amplifier. Would you guys have anything that is a direct replacment for the below? It would have to be High temperature…
Tool/software:
Hi,
This is related to my previous thread on OPA211-HT
I have the following questions:
1. Since Ios at 210 C is 150 nA(max) and I am using this op amp at 210C, with gain of about 700, should I be concerned about…
Tool/software:
We intend to use this op amp (OPA211-HT) in our pressure transducer, which needs to operate at around 250 C temperature. The parameters such as: open loop gain, Vos, Ib are reasonable (compared to other high temp…
Hello,
I am using "OPA211-HT" (since it is available in KGD form). With unity gain for input voltage from 0 to 3.3V, I get linear output. But when I set gain to 4.16, I see non liner behavior for input voltage below 1.25V…
We are using your 200 °C integrated components with HKQ case(OPA211SHKQ). These components have a space of 1 / 1.3mm in the part below in contact with the PCB.Does this space need to be filled with a resin to firmly fix the components…
Hi Team,
Is there TI solution to replace ADI AD8634HRZN? AD8634HRZN temperature is -40C to 175C, however OPA2210IDR only up to 125C.
Please suggest. Thanks.