Tool/software:

Tool/software:
Tool/software:
I have a Raspberry Pi camera module 2 (IMX219). How can I use it with the AM62A SK EVM?
Tool/software:
Hey all,
If someone could idiot-proof this for me I'd be grateful.
1. Can I output pwm on the 4 mcu+ timers?
2. I read that there can be resource reallocation…
Tool/software:
Hi,
I tested with AM62A PSDK 10.01.00.05, and the sigmoid issue occurred again.
The issue occurs in one of the multiple sigmoid layers.
Here are…
Tool/software:
Tool/software:
Hello Team,
I am using gstreamer pipeline to stream h264 data. for that, I am using v4l2h264enc plugin.
Command:
gst-launch-1.0 -v v4l2src device=/dev/video-rpi-cam0 io-mode=dmabuf-import ! video/x-bayer, width=1920…
Tool/software:
Hello Expert,
How can I modify or disable UI and make the screen shows only CLI.
Warm Regards,
Sajan
Tool/software:
Help with Real-Time Model Deployment and Network Streaming on AM62A LP
Hi,
I am working with the AM62A LP board and would like to load my custom machine learning model onto the board. My goal is to achieve real…
Tool/software:
Hello,
we want to use use gstreamer pipeline from within docker on target. Gst plugins like tiovx should be useable.
Are there any ready docker images for target availbale?
If not, how to create docker image for…
Tool/software:
I need to connect 6 SPST Normally Open switches to the SK-AM62A-LP directly to the AM62 processor.
Which pins are free to use?
For some reason, the pins on the TM4C1294NCPDTT3R…