Tool/software:
#include <iostream> #include "opencv2/opencv.hpp" #include "opencv2/core.hpp" #include "opencv2/imgproc.hpp" using namespace std; int main( ) { cv::Mat image = cv::Mat::ones(500, 500, CV_8UC3) * 255; std::string text = "Hello, World!"; cv::Point position(100, 250); int font = cv::FONT_HERSHEY_SIMPLEX; cv::Scalar color(0, 0, 0); cv::putText(image, text, position, font, 1.5 , color, 2); cv::imwrite("./test.jpg", image); }
Hello,
OpenCV installed in the SDK should be sufficient for an example like this. I would be curious to see your CMakeLists.txt file for this project -- would you please share this?
A good example is under edgeai-tidl-tools --- see examples. Within the osrt_cpp examples, you can see several instances in which imwrite is used:
It is an option to cross-compile, but this is not required here. The necessary headers, libraries, and compiler are present in the SDK within /usr. Yocto is used to create the distribution of Linux, so all the packages, tools, libraries, configurations, and so on -- it is not the right tool for your use-case here.
Are you using edgeai-gst-apps as your starting point for this application? I see similarities in the directory structure with apps_cpp. That project (under /opt/edgeai-gst-apps/apps_cpp) builds without any of these linking issues.
BR,
Reese
Hello, I don't know how to use edgeai-gst-apps as the starting point of the application. Where can I refer to it?
The project I tested before was Hello world, which can be compiled and executed on the board according to the following steps:
1) mkdir build
2) cd build
3) cmake ..
4) make
The code structure is as follows:
The content of CMakeLists.txt in the APPS_CPP/folder is as follows:
The content of CMakeLists.txt in the APPS_CPP/app_edgeai/src directory is as follows:
This is our CMakeLists, please take a look, looking forward to your reply.
I don't know how to use edgeai-gst-apps as the starting point of the application. Where can I refer to it?
I made an assumption based on your directory structure that you had used edgeai-gst-apps at first, and were using the common.cmake from there. I think I made an incorrect assumption here.
For a hello-world style application, edgeai-gst-apps may be overly complex. However, it has a common.cmake file that may be useful -- it sets Library and Include paths that are known to work.
Could you also share the common.cmake? The cmake files you shared do not include any of the right libraries or include paths, so I assume it exists in the common.cmake file.
I assume you are compiling on the target. Please tell me if this is incorrect.
BR,
Reese
Hello, this is our common.cmake file; the location is as follows:
The specific content is as follows:
include(GNUInstallDirs) include(CMakePackageConfigHelpers) add_compile_options(-std=c++17) option(USE_DLR_RT "Enable DLR inference" ON) option(USE_TENSORFLOW_RT "Enable Tensorflow inference" ON) option(USE_ONNX_RT "Enable Onnx inference" ON) # Specific compile optios across all targets #add_compile_definitions(MINIMAL_LOGGING) IF(NOT CMAKE_BUILD_TYPE) SET(CMAKE_BUILD_TYPE Release) ENDIF() # Turn off output data dumps for testing by default OPTION(EDGEAI_ENABLE_OUTPUT_FOR_TEST "Enable Output Dumps for test" OFF) # Check if we got an option from command line if(EDGEAI_ENABLE_OUTPUT_FOR_TEST) message("EDGEAI_ENABLE_OUTPUT_FOR_TEST enabled") add_definitions(-DEDGEAI_ENABLE_OUTPUT_FOR_TEST) endif() message(STATUS "CMAKE_BUILD_TYPE = ${CMAKE_BUILD_TYPE} PROJECT_NAME = ${PROJECT_NAME}") SET(CMAKE_FIND_LIBRARY_PREFIXES "" "lib") SET(CMAKE_FIND_LIBRARY_SUFFIXES ".a" ".lib" ".so") if(NOT CMAKE_OUTPUT_DIR) set(CMAKE_OUTPUT_DIR ${CMAKE_SOURCE_DIR}) endif() set(CMAKE_ARCHIVE_OUTPUT_DIRECTORY ${CMAKE_OUTPUT_DIR}/lib/${CMAKE_BUILD_TYPE}) set(CMAKE_LIBRARY_OUTPUT_DIRECTORY ${CMAKE_OUTPUT_DIR}/lib/${CMAKE_BUILD_TYPE}) set(CMAKE_RUNTIME_OUTPUT_DIRECTORY ${CMAKE_OUTPUT_DIR}/bin/${CMAKE_BUILD_TYPE}) if (NOT DEFINED ENV{SOC}) message(FATAL_ERROR "SOC not defined.") endif() set(TARGET_SOC_LOWER $ENV{SOC}) if ("${TARGET_SOC_LOWER}" STREQUAL "j721e") set(TARGET_PLATFORM J7) set(TARGET_CPU A72) set(TARGET_OS LINUX) set(TARGET_SOC J721E) elseif ("${TARGET_SOC_LOWER}" STREQUAL "j721s2") set(TARGET_PLATFORM J7) set(TARGET_CPU A72) set(TARGET_OS LINUX) set(TARGET_SOC J721S2) elseif ("${TARGET_SOC_LOWER}" STREQUAL "j784s4") set(TARGET_PLATFORM J7) set(TARGET_CPU A72) set(TARGET_OS LINUX) set(TARGET_SOC J784S4) elseif ("${TARGET_SOC_LOWER}" STREQUAL "j722s") set(TARGET_PLATFORM J7) set(TARGET_CPU A53) set(TARGET_OS LINUX) set(TARGET_SOC J722S) elseif ("${TARGET_SOC_LOWER}" STREQUAL "am62a") set(TARGET_PLATFORM SITARA) set(TARGET_CPU A53) set(TARGET_OS LINUX) set(TARGET_SOC AM62A) elseif ("${TARGET_SOC_LOWER}" STREQUAL "am62x") set(TARGET_PLATFORM SITARA) set(TARGET_CPU A53) set(TARGET_OS LINUX) set(TARGET_SOC AM62X) elseif ("${TARGET_SOC_LOWER}" STREQUAL "am62p") set(TARGET_PLATFORM SITARA) set(TARGET_CPU A53) set(TARGET_OS LINUX) set(TARGET_SOC AM62P) else() message(FATAL_ERROR "SOC ${TARGET_SOC_LOWER} is not supported.") endif() message("SOC=${TARGET_SOC_LOWER}") add_definitions( -DTARGET_CPU=${TARGET_CPU} -DTARGET_OS=${TARGET_OS} -DSOC_${TARGET_SOC} ) set(TENSORFLOW_INSTALL_DIR ${TARGET_FS}/usr/include/tensorflow) set(ONNXRT_INSTALL_DIR ${TARGET_FS}/usr/include/onnxruntime) set(TFLITE_INSTALL_DIR ${TARGET_FS}/usr/lib/tflite_2.12) if(USE_DLR_RT) add_definitions(-DUSE_DLR_RT) endif() if(USE_TENSORFLOW_RT) add_definitions(-DUSE_TENSORFLOW_RT) endif() if(USE_ONNX_RT) add_definitions(-DUSE_ONNX_RT) endif() link_directories(${TARGET_FS}/usr/lib/aarch64-linux-gnu ${TARGET_FS}/usr/lib/ ) if(USE_DLR_RT) link_directories(${TARGET_FS}/usr/lib/python3.12/site-packages/dlr) endif() if(USE_TENSORFLOW_RT) link_directories(${TFLITE_INSTALL_DIR}/ruy-build ${TFLITE_INSTALL_DIR}/xnnpack-build ${TFLITE_INSTALL_DIR}/pthreadpool ${TFLITE_INSTALL_DIR}/fft2d-build ${TFLITE_INSTALL_DIR}/cpuinfo-build ${TFLITE_INSTALL_DIR}/flatbuffers-build ${TFLITE_INSTALL_DIR}/abseil-cpp-build ${TFLITE_INSTALL_DIR}/farmhash-build ) endif() if(USE_ONNX_RT) endif() #message("PROJECT_SOURCE_DIR =" ${PROJECT_SOURCE_DIR}) #message("CMAKE_SOURCE_DIR =" ${CMAKE_SOURCE_DIR}) include_directories(${PROJECT_SOURCE_DIR} ${PROJECT_SOURCE_DIR}/.. ${PROJECT_SOURCE_DIR}/include SYSTEM ${TARGET_FS}/usr/local/include SYSTEM ${TARGET_FS}/usr/include/gstreamer-1.0 SYSTEM ${TARGET_FS}/usr/include/glib-2.0 SYSTEM ${TARGET_FS}/usr/lib/glib-2.0/include SYSTEM ${TARGET_FS}/usr/lib/aarch64-linux-gnu/glib-2.0/include SYSTEM ${TARGET_FS}/usr/include/opencv4/ SYSTEM ${TARGET_FS}/usr/include/processor_sdk/vision_apps SYSTEM ${TARGET_FS}/usr/include/processor_sdk/app_utils SYSTEM ${TARGET_FS}/usr/include/edgeai_dl_inferer ) if(USE_DLR_RT) include_directories(${TARGET_FS}/usr/lib/python3.12/site-packages/dlr/include/) endif() if(USE_TENSORFLOW_RT) include_directories(SYSTEM ${TENSORFLOW_INSTALL_DIR} SYSTEM ${TENSORFLOW_INSTALL_DIR}/lite/tools/make/downloads/flatbuffers/include ) endif() if(USE_ONNX_RT) include_directories(SYSTEM ${ONNXRT_INSTALL_DIR}/include/onnxruntime SYSTEM ${ONNXRT_INSTALL_DIR}/include/onnxruntime/core/session ) endif() set(COMMON_LINK_LIBS ################################################################################### #our .so/.a libs file ################################################################################### ) set(SYSTEM_LINK_LIBS ncurses tinfo gstreamer-1.0 glib-2.0 gobject-2.0 gstapp-1.0 opencv_core opencv_imgproc yaml-cpp pthread dl ) if(NOT ${TARGET_SOC} STREQUAL "AM62X" AND NOT ${TARGET_SOC} STREQUAL "AM62P") set(SYSTEM_LINK_LIBS ${SYSTEM_LINK_LIBS} tivision_apps) endif() if(USE_DLR_RT) set(SYSTEM_LINK_LIBS ${SYSTEM_LINK_LIBS} dlr) endif() if(USE_TENSORFLOW_RT) set(SYSTEM_LINK_LIBS ${SYSTEM_LINK_LIBS} tensorflow-lite) set(SYSTEM_LINK_LIBS ${SYSTEM_LINK_LIBS} flatbuffers fft2d_fftsg2d fft2d_fftsg cpuinfo farmhash ruy_allocator ruy_apply_multiplier ruy_blocking_counter ruy_block_map ruy_context ruy_context_get_ctx ruy_cpuinfo ruy_ctx ruy_denormal ruy_frontend ruy_have_built_path_for_avx2_fma ruy_have_built_path_for_avx512 ruy_have_built_path_for_avx ruy_kernel_arm ruy_kernel_avx2_fma ruy_kernel_avx512 ruy_kernel_avx ruy_pack_arm ruy_pack_avx2_fma ruy_pack_avx512 ruy_pack_avx ruy_prepacked_cache ruy_prepare_packed_matrices ruy_system_aligned_alloc ruy_thread_pool ruy_trmul ruy_tune ruy_wait pthreadpool XNNPACK ) endif() if(USE_ONNX_RT) set(SYSTEM_LINK_LIBS ${SYSTEM_LINK_LIBS} onnxruntime) endif() set(SYSTEM_LINK_LIBS ${SYSTEM_LINK_LIBS} pthread dl) # Function for building a node: # ARG0: app name # ARG1: source list function(build_app) set(app ${ARGV0}) set(src ${ARGV1}) add_executable(${app} ${${src}}) target_link_libraries(${app} -Wl,--start-group ${COMMON_LINK_LIBS} ${TARGET_LINK_LIBS} ${SYSTEM_LINK_LIBS} -Wl,--end-group) endfunction(build_app) # Function for building a node: # ARG0: lib name # ARG1: source list # ARG2: type (STATIC, SHARED) function(build_lib) set(lib ${ARGV0}) set(src ${ARGV1}) set(type ${ARGV2}) set(version 1.0.0) add_library(${lib} ${type} ${${src}}) get_filename_component(PROJ_DIR "${CMAKE_CURRENT_SOURCE_DIR}" NAME) set(INC_DIR_DST ${CMAKE_INSTALL_LIBDIR}/${CMAKE_INSTALL_INCLUDEDIR}/${PROJ_DIR}) install(TARGETS ${lib} LIBRARY DESTINATION ${CMAKE_INSTALL_LIBDIR} # Shared Libs ARCHIVE DESTINATION ${CMAKE_INSTALL_LIBDIR} # Static Libs RUNTIME DESTINATION ${CMAKE_INSTALL_BINDIR} # Executables, DLLs INCLUDES DESTINATION ${INC_DIR_DST} ) # Specify the header files to install install(DIRECTORY ${CMAKE_CURRENT_SOURCE_DIR}/include DESTINATION ${INC_DIR_DST} ) endfunction(build_lib)
Please help me take a look, thank you very much!
Hello,
The CMAKE file here is helpful. I think the issue is with the set of linked libraries. Here, you are adding (from opencv) core and imgproc libraries, but I don't think this contains the imwrite function.
It looks like imwrite is part of libopencv_imgcodecs. Could you try adding "opencv_imgcodecs" to your SYSTEM_LINK_LIBS (line 170)?
As a quick check, I dumped symbols with "nm -D" for the libopencv_core.so, libopencv_imgproc.so, and libopencv_imgcodecs.so:
root@am62axx-evm:/usr/lib# nm -D libopencv_core.so | grep imwrite root@am62axx-evm:/usr/lib# nm -D libopencv_imgproc.so | grep imwrite root@am62axx-evm:/usr/lib# nm -D libopencv_imgcodecs.so | grep imwrite 000000000002a900 T _ZN2cv7imwriteERKNSt7__cxx1112basic_stringIcSt11char_traitsIcESaIcEEERKNS_11_InputArrayERKSt6vectorIiSaIiEE
And it is defined only in imgcodecs
BR,
Reese