Part Number: PROCESSOR-SDK-AM62A
Tool/software:
I currently have an AM62A development board with system SDK 9.2. The model has been successfully converted and deployed on the board, and it can run correctly to produce the expected results. However, I encountered an issue: during model inference, if the program crashes or is forcefully terminated (e.g., using Ctrl+C), in short, if the resource release code is not executed properly, the model cannot run correctly the next time. The only solution is to restart the board. The error message is as follows:
libtidl_onnxrt_EP loaded 0xed32db0
Final number of subgraphs created are : 1, - Offloaded Nodes - 132, Total Nodes - 135
176789.252347 s: VX_ZONE_ERROR:[ownContextSendCmd:875] Command ack message returned failure cmd_status: -1
176789.252405 s: VX_ZONE_ERROR:[ownNodeKernelInit:590] Target kernel, TIVX_CMD_NODE_CREATE failed for node TIDLNode
176789.252424 s: VX_ZONE_ERROR:[ownNodeKernelInit:591] Please be sure the target callbacks have been registered for this core
176789.252439 s: VX_ZONE_ERROR:[ownNodeKernelInit:592] If the target callbacks have been registered, please ensure no errors are occurring within the create callback of this kernel
176789.252457 s: VX_ZONE_ERROR:[ownGraphNodeKernelInit:608] kernel init for node 0, kernel com.ti.tidl:1:1 ... failed !!!
176789.252487 s: VX_ZONE_ERROR:[vxVerifyGraph:2159] Node kernel init failed
176789.252500 s: VX_ZONE_ERROR:[vxVerifyGraph:2213] Graph verify failed
TIDL_RT_OVX: ERROR: Verifying TIDL graph ... Failed !!!
TIDL_RT_OVX: ERROR: Verify OpenVX graph failed
After investigation and preliminary analysis, it is determined that TI's model inference does not directly invoke the hardware but instead communicates with other processes, which are responsible for resource allocation. When the program crashes, it fails to send the release signal to the corresponding process, resulting in resource occupation. This lack of available resources leads to errors when attempting to run the model again.
[C7x_1 ] 28392.238061 s: IPC: Echo status: a530-0[.] r5f0-0[P] c75ss0[s]
[C7x_1 ] 176789.251932 s: VX_ZONE_ERROR:[tivxAlgiVisionAllocMem:194] Failed to Allocate memory record 13 @ space = 17 and size = 4964028 !!!
[C7x_1 ] 176789.251968 s: VX_ZONE_ERROR:[tivxAlgiVisionCreate:358] tivxAlgiVisionAllocMem Failed
[C7x_1 ] 176789.251999 s: VX_ZONE_ERROR:[tivxKernelTIDLCreate:926] tivxAlgiVisionCreate returned NULL
[C7x_1 ] 176789.548018 s: VX_ZONE_ERROR:[tivxAlgiVisionAllocMem:194] Failed to Allocate memory record 13 @ space = 17 and size = 3828764 !!!
[C7x_1 ] 176789.548052 s: VX_ZONE_ERROR:[tivxAlgiVisionCreate:358] tivxAlgiVisionAllocMem Failed
[C7x_1 ] 176789.548082 s: VX_ZONE_ERROR:[tivxKernelTIDLCreate:926] tivxAlgiVisionCreate returned NULL
[C7x_1 ] 176789.860206 s: VX_ZONE_ERROR:[tivxAlgiVisionAllocMem:194] Failed to Allocate memory record 5 @ space = 17 and size = 2935104 !!!
[C7x_1 ] 176789.860240 s: VX_ZONE_ERROR:[tivxAlgiVisionCreate:358] tivxAlgiVisionAllocMem Failed
[C7x_1 ] 176789.860269 s: VX_ZONE_ERROR:[tivxKernelTIDLCreate:926] tivxAlgiVisionCreate returned NULL
[C7x_1 ] 176790.194297 s: VX_ZONE_ERROR:[tivxAlgiVisionAllocMem:194] Failed to Allocate memory record 5 @ space = 17 and size = 2826986 !!!
[C7x_1 ] 176790.194331 s: VX_ZONE_ERROR:[tivxAlgiVisionCreate:358] tivxAlgiVisionAllocMem Failed
[C7x_1 ] 176790.194361 s: VX_ZONE_ERROR:[tivxKernelTIDLCreate:926] tivxAlgiVisionCreate returned NULL
Is there any API available to manually release these resources? Or, how can this issue be effectively resolved?