Other Parts Discussed in Thread: TLC59283
Tool/software:
Hello everyone! New to the forum here. Sorry if the part is wrong but apparently I can only choose power managment subforum with this IC.
I'm designing a led driver with TLC59283…
Hello,
I have a TLC59283 application whereby some of the channels are 3 LEDs in series (Vf = 2.1V each for a total of 6.2V) but others are only 1 LED (Vf total of 2.1V). I saw that the maximum LED voltage for this part is 10V, but…
Hi team,
How can I deal with unused output of TLC59283, like pin 19? Just floating?
Regards,
Xiaoying
Hello,
I'm using a few TLC59283 ICs to drive seven segment displays, HDSP-521G, Vf = 2.0V. For highest efficiency and least heating of the TLC59283, what would be the best voltage to supply the LED displays with? 3.3V or 5.0V…
Good afternoon,
I am looking to drive 4x 7-segment displays using the TLC59283. The TLC59283 is driven by a synchronous serial interface, should I use one of the MSP432E401Y's SPI channels…
Hi,
we are updating a legacy design where the GND connection of the TLC59283 (pin 22 in the QFN-24 package) is being filtered (probably for EMI reasons). In that design the thermal pad is connected to the same net, which means the…
Hi,
My customer is using TLC59283 as LED driver. However, they are facing an EMI problem so I reach out to you for some help.
Noise is detected in 23Mhz and 46Mhz when the LED is on, however when the LED is turned off the noise disappears…
Hello experts,
I have question for total current capability. TLC59283 can drive max 45mAx16ch = 720mA if we ignore thermal problem? Or is ther any total current limit as device?
Thanks and best regards,
Ryo Akashi
Hi.
I want to use some daisy-chained TLC59283 and also need dimming.
At the first time I designed with some 74LV595A, but I need to minimize space on…
Hi,
Can you suggest how to select zener in the resistor-zener circuitry for ghost cancellation