Hello,
I have a TLC59283 application whereby some of the channels are 3 LEDs in series (Vf = 2.1V each for a total of 6.2V) but others are only 1 LED (Vf total of 2.1V). I saw that the maximum LED voltage for this part is 10V, but can I supply the anode of some channels with 7V and others with 3V? That would be more efficient than using 7V for all channels.
Thanks,
Derek