Part Number: ADS1000-Q1 Looking at DS REV B OCT2015, just want confirm if the absolute maximum rating on item "Voltage to GND, VIN+, VIN-" is VDD+0.3 instead of just "0.3"
Part Number: ADS1000-Q1ADS1000-Q1 is used for NTC resistance temperature detection. The current connection method is single power supply.
How can the output of ADS 1000-Q1 be converted into voltage value? Is there a conversion formula or detailed documentation…
Part Number: ADS1000-Q1 Other Parts Discussed in Thread: ADS1000 Hi Team,
Is it ok to drive the ADS1000-Q1 with a high Z input 10kOhm range?
Thanks, Mitchell
Part Number: ADS1000-Q1 Other Parts Discussed in Thread: ADS1000 Tool/software: Code Composer Studio Hello,
In our project, ads1000-q1 chip is used
The usage is shown in the attachment. When the display screen is connected to ads1000-q1, the display temperature…
Part Number: ADS1000-Q1 Hi team,
Could you please help to check if we could use 10nF filter cap on VIN+ in single ended input application?
Also any problem for below SCH?
Other Parts Discussed in Thread: ADS1000-Q1 Hi There,
My customer is running the ADS1000-Q1 from 2.8V. However the i2c address does not appear to ACK. Other devices running off the bus are operating as expected. The customer is yet to try a bus interrogation…
Thank you sir,
i am using ADS1000-Q1 (www.ti.com/.../ADS1000-Q1) BYMQ - Slave Address 1001001 . circuit diagram same as you given.
Master send 0x93H address will not getting acknowledgement . if maser send (General Call data bytes) 0x04H Or 0x06H …