Part Number: ADS1120-Q1 Tool/software: Hi team,
When the ADS1120-Q1 is powered on, the ADC sampling fails.
Fault description: Our software will send a reset command to the ADC chip via SPI when powered on, set the value of the 02h register to 0x10, and…
Part Number: ADS1120-Q1 Hi team,
Could you please help give some comments about the following questions? Thank you!
My customer is using the ADS1120-Q1 in the project, the power supply is CR2032b, voltage 2v~3V. The bridge parameters are:
Piezo resistance…
Part Number: ADS1120-Q1 Other Parts Discussed in Thread: ADS1120 , Hello
I am using STM32L series micro controller in my project and using ADS1120 in continuous conversion mode(not using the DRDY pin).
Is there a sample C code available to start with other…
Part Number: ADS1120-Q1 Hello
I have been using ADS1120-Q1 for reading an analog voltage on the IN0 pin vs AVSS (IN1,IN2,IN3,REFN0,REFP0,DRDY are left unused & VA is fed 5V & CLK pin is tied to GND) & the configuration registers are set as below:…
Part Number: ADS1120-Q1 Hey Matt.
Its been long while .. What's up.. How are you ?? I have been using the ADS1120-Q1 for my current measurement . I have tried with the two different register 2 configuration. One with the VREF as : Analog supply (AVDD…
Part Number: ADS1120-Q1 Other Parts Discussed in Thread: ADS131B04-Q1 Hi Team,
At presently in our products, for sensing application we are using ADS1120-Q1 16 bit ADC converter, it is working fine and we are able to get the data as well, but the sensing…
Part Number: ADS1120-Q1 Other Parts Discussed in Thread: ADS1120 , , ADS131B02-Q1 I want to use the differential input port of ads1120 as the input of both side of the shunt sampling resistor( range ±100mV), but I only have a positive power supply externally…
Part Number: ADS1120-Q1 HI Team,
8.3.11 System Monitor of the datasheet says:"Note that the system monitor function only provides a coarse result and is not meant to be a precision measurement"
Could you please provide the acuracy data of measuring…
Part Number: ADS114S08 Other Parts Discussed in Thread: ADS1120-Q1 , ADS1148-Q1 , ADS1261-Q1 , ADS1018-Q1 , LMP90080-Q1
Tool/software:
Hi, I need to know if this ADC ADS114S0x Low-Power, Low-Noise, Highly Integrated, 6- and 12-Channel, 4-kSPS, 16-Bit, Delta…
Hi Furqan,
ADS112U04 and ADS122U04 are our only UART interface ADCs, and these are only available in Catalog Rating.
Our most comparable device with Automotive Rating would be ADS1120-Q1 data sheet, product information and support | TI.com .
This device…