Part Number: ADS1293 Can I use a single ADS1293 for 12 lead egc measurement by multiplexing 10 egc leads using analogue multiplexer. 3 Channel reading at a time 7 then switch over of electrodes. total 3 set of measurement for 12 lead measurement
Part Number: ADS1293 We have designed the EMG design for the ADS1293 along with the input opamp of gain 500 to 1000.
I just want to review the schematics design since the flow is like electrodes-->> Opamp -->> ADS1293 whether for 2-channel data acquisition…
Part Number: ADS1293 R2 = 6, R3 = 16, ADCmax = 0xF30000, sample rate = 267
I am not sure what raw ADC value you get with a +5mV input. Is the raw value a signed number? If I put zero volts into the ADCout equation , I get 0.5 * ADCmax = 7,962,624.
…
Part Number: ADS1293 I want to reduce power consuption during off state of the device
Can I reduce VDD (V to the analog part to zero while VDDIO (V to digital part is 3V)?
what is the best way to put the ADS1293 in low power mode
thanks
avihoo keret
Part Number: CC2650MODA Other Parts Discussed in Thread: ADS1293 , CC2650 Hello d ear TI rep, I would like to modify the CC2650 sensor tag code to integrate with ADS1293 via SPI available. What readily ADS1293 code resources available that we can use to…
Part Number: ADS1293
I am in the process of doing the IEC-60601-2-47.
I am trying to apply the 300mv offset to the ECG inputs via the S3 switch in the test circuit. Does anyone know what this 300mV is referenced to. It just shows the recorder.
Is it…
Part Number: ADS1292 Other Parts Discussed in Thread: ADS1293 , , ADS1294R I have a system that uses the ads1293 and it works well. I want to add respiration so I want to
run a 1292R chip in sync with the 1293..
I this possible ? is it a good idea ?
The…
Part Number: ADS1293 We have DC LOD detect enabled and when the current is set above 120nA the Lead off detect work great. However when we run the impedance test for IEC60601-2-27 Section 201.12.1.101.3, we get a flat line. Only when we lower the current…
Part Number: ADS1293 Hi TI,
we are using the ADS1293 without an RLD and want to use a Lead-off detection. I read this post in your forum and will try this ways.
https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/1245713…
Part Number: ADS1293 Other Parts Discussed in Thread: ADS1294R
I have developed a 3-channel ECG monitor utilizing the ADS1293. It is functioning properly. However, as it is a wearable device, it is encountering significant noise issues, including powerline…