Part Number: ADS131M08EVM Other Parts Discussed in Thread: TLV2252 Hi TI,
I am trying to measure the output voltage of a medical oxygen sensor (PN: OOM102-1).
The relative information is highlighted below:
Output voltage: 9~14 mV
Recommended load: >=…
Part Number: ADS131M08EVM Other Parts Discussed in Thread: ADS131M08 We purchased 2x ads131m08evm. Is it possible to connect two modules to the same computer for data collection using the GUI?
We ultimately plan to communicate with the modules via SPI…
Part Number: ADS131M08EVM Can TI share the labview drivers/VI's for the ADS...EVM board ecosystem?
It would enable developers to validate a design using Labview.
Part Number: ADS131M08EVM Other Parts Discussed in Thread: ADS131M08 , Hi,
I have purchased the ADS131M08EVM development board so I can analyze the ADS131M08 ADC for current and future products. I have read the datasheet and it looks like I should be using…
Part Number: ADS131M08EVM
Hello,
I´m using in my application an ADS131M08EVM with an MCU STM32. The SPI communication is already happening correctly, but the readings aren´t precise due to the lack of calibration of the channels. I would like…
Part Number: ADS131M08EVM Other Parts Discussed in Thread: ADS131M08 , ADS131M06 Hello everyone, hope you are well!
Me and my team are developing an energy meter using an MCU STM32F756ZG with HAL Library and an ADS131M08EVM to acquire the signals.
We were…
Part Number: ADS131M08EVM Other Parts Discussed in Thread: ADS131M08 Hi,
I am using an ADS131M08EVM to measure the output from an analog +/- 3 g triaxial accelerometer that outputs 0 to about 3.3 V. At 0 g the output is about 1.65 V. What is the proper…
Part Number: ADS131M08EVM Hi,
I'm using a load cell with these specifications:
Full-scale load: 4400N
Rated Output; 4.5mv/v
Excitation: max 15.
ADC res, 24 Bit
I want to have a minimum 10N accuracy. I connected to excitation to a 2.5V accurate reference…
Part Number: ADS131M08EVM Other Parts Discussed in Thread: ADS131M08 , , ADS131A04
All:
I have been able to install the EVM support software on my computer.
If I want to run the ADS131M08 that is on the EVM from a different microcontroller, is there…
Part Number: ADS131M08EVM Hii.
It looks like the EVM GUI does provide continuous save to file for samples , but only in small 16384KB files.
Is this expected ?
Pierre