Part Number: ADS4245EVM Trying to locate the ADS4245EVM and TSW1400EVM. Are there any in existence? are there replacement/ recommended EVM's similar for these evaluation boards?
This is being addressed at another forum post
https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/1305368/ads4245-ads4245evm
Hello
Jae-heung Yeom said: 2. ADS42xx GUI does not connect to ADS4245EVM.
The USB Status light is dark and the values are not applied.
How can I know GUI is connected to ADS4245EVM?
Is there any method to change the ADS4245 register?
You should be able…
Part Number: ADS4245EVM Other Parts Discussed in Thread: ADS4245 Hello,
My customer wants to test the ADS4245EVM after purchasing it.
The ADS4245EVM webpage on TI.com states that it is directly compatible with the TSW1400EVM and TSW1405EVM, but they cannot…
Part Number: ADS4245EVM
Originally the ADS4245EVM board is configured to work for only ac signals above 0.5 MHz. I wanted it to work for lower frequencies also. Starting from DC.
So I made a following change in the circuit.
However the signal…
Part Number: ADS4245EVM Other Parts Discussed in Thread: SN74AVC16T245 I bought a new board a few days back and the board is not giving out any signal
I have given the board the required 5 V. The RESET pin is high. The SCLK pin is HIGH. The SEN pin is…
Part Number: AFE5808AEVM Other Parts Discussed in Thread: ADS4245EVM , AFE5818 , AFE58JD18 Hi, we have a AFE5808AEVM and tried to order the partner capture board TSW1400EVM but it is obsolete and unavailable. I have been trying though our supply chain since…
Part Number: ADS4249EVM Other Parts Discussed in Thread: ADS4245EVM , ADS4245 I am interested in evaluating the ADS4245. I cannot, however, locate any stock of the ADS4245EVM. I do locate stock of ADS4249EVM. It appears these two eval platforms are based…
Other Parts Discussed in Thread: ADS4245EVM Recently purchased an ADS4245EVM module and a TSW1400EVM High Speed Data Capture Card to go with it. The integrated platform is working with the installed High Speed Data Converter Pro SW. However, controlling…
Other Parts Discussed in Thread: ADS4245 , SN74AVC16T245 , ADS4245EVM Hello,
I have an ADS4245 EVM. I want to use CMOS mode on this board which output from J1. In order to use CMOS mode, I just follow the datasheet 'User's Guide ADS42xx EVM' on page…