Part Number: TSW1400EVM
Hi Team,
Our customer would like to control DAC5681 and ADS5463EVM simultaneously with the HSDC GUI. According to our customer,
We have tested successfully the TSW1400 module, controlled by the HSDC pro GUI separately with a DAC5681…
Part Number: ADS5463EVM Other Parts Discussed in Thread: ADS5463 , ADS4249 I am using ADS5463EVM with 12 bit LVDS signals. Do you have perhaps a VHDL core for this LVDS transmiton? DDR or SDR are both great, but not serdess, as it is data receive with…
Hi Hirano-san,
Using our ADS5463EVM-CVAL, I applied a 100 MSPS clock and 301 MHz input driven to -0.95 dBFs. The power supplies current were as follows:
5V AVDD: 290.6 mA
3.3V AVDD:133.2 mA
3.3V DVDD: 80.4 mA
This is roughly 2.158 W
Best regards,
Dre…
Hi Jim,
I could capture ADC output for 400Mhz with static timing solution. now I am going to capture with 500Mhz But for 500Mhz static timing dose not work and I have to use dynamic calibration to capture the proper data, I don't have any idea about dynamic…
Part Number: ADS5463EVM Other Parts Discussed in Thread: DAC3152EVM
I am planning to use Xilinx ZC706 with TI based ADC and DAC EVM boards ADS5463EVM and DAC3152EVM for my design. I want my system to be clock synchronous (synchronized clock for ADC, DAC…
Part Number: ADS5463EVM Other Parts Discussed in Thread: ADS5463 , CDCM7005 , LMX2582EVM Hi,
I have some question about your ADS5463EVM, I have this evaluation board now, bout I have some problem with input frequency. according ADS5463 datasheet this chip…
Part Number: ADS5463EVM Hi there,
I am using ADS5463EVM to capture ADC data with ZYNQ Z7020, I have got ADC data with 400Mhz (200Mhz DDR) for input 25Mhz sine wave with static capture . But I want to capture 30Mhz input sine wave, then I have to increase…
Part Number: ADS5463EVM Other Parts Discussed in Thread: DAC3161EVM , FMC-DAC-ADAPTER , DAC3161 , ADS5463 , CDCM7005 , DAC3162EVM What is needed to connect these 2 Evms without an fpga ?
I need to connect them as a proof of concept with a simple connector…
Part Number: ADS5463EVM Other Parts Discussed in Thread: ADS5463 , ADS4249 I am developing RF sampler using ADS5463EVM and I am using DE-2 115 Altera FPGA board. I wanted to get VHDL code for data communication via ADC-HSMC(Altera) header adapter card…
Other Parts Discussed in Thread: ADS5463EVM Can anyone please share the dimensions of the ADS5463EVM evaluation board?
Does anyone have the Gerber files for this board?