Part Number: ADS6125 Hi team,
Is there away to interface linux board with ADS6125? If it can be interfaced, what communication port I should use, SPI?
How to acquire the ADC data and put into the DMA. After that how can I use the poll() function to read…
Part Number: ADS6125 Hi Team, we would like to confirm when is an acceptable range of time from our external clock rising edge (54Mhz clock) to when the input data can be sampled in the FPGA?
Thank you for your inputs.
Regards,
Mark
Part Number: ADS6125 Hi Team, Posting on behalf of our customer. They intend to operate ADS6125 in parallel CMOS but the datasheet apparently lacks information on the reason the external clock is preferred to use over CLKOUT at DRVDD < 2.2V. Currently they…
Part Number: ADS6125 In ADS6125 data sheet the transformer WBC1-1 is recommended and in ADS6125 EVM the TC1-4W is recommended. Which one should I choose?
Part Number: ADS6125 Other Parts Discussed in Thread: LMX2571 , I'm going to select LMX2571 as the clock generator. LMX2571 has tow options outputting clock - open drain and push pull. Regarding ADS6125 which type output is selected?
Part Number: ADS6125 In CMOS MODE, selecting the serial interface, only programming PDN in registers and not connecting the PDN pin in hardware. Is it correct?
In ADS6125 EVM the OVR is not used. Is it?
Part Number: ADS6125 Other Parts Discussed in Thread: LMK04208 , DAC7760 , I'm going to design a shared power supply i.e. ADS6125, DAC7760 and LMK04208 will share a power supply. The load 1 is ADS7760. Is it ok?
Part Number: ADS6125 Other Parts Discussed in Thread: TPS82085 , , TSW40RF80EVM Do AVDD and DRVDD power suppliers require LDO? I have not foun out the power supply recommendation from the data sheet.