Hello,
unfortunately there is no a Verilog model nor sample code for this device.
There is an IBIS model, and TINA spice mode available for the device in the Design and Development Tab of the product folder.
If you encounter any issues, please post and…
Part Number: ADS8638EVM-PDK Hello, I have recently purchased a ADS8638EVM-PDK but the documentation does not include schematics (despite saying that it does!)
Please can someone send me the schematics for this board, and also for the baseboard that it…
Part Number: ADS8638EVM-PDK Other Parts Discussed in Thread: ADS8638 Hello,
I am using the ADS8638EVM-PDK along with the MMB0 base-board for evaluation of the ADS8638.
Do I need to use a separate power supply to power the chips HVDD and HVSS pins? Looking…
Hello
ADS8638EVM-PDK: Can I get a FPGA source (Verilog) code for ADS8638?
or ADS8568EVM-PDK: Can I get a FPGA source (Verilog) code for ADS8568?
Because currently using ADS8638, so try to provide ADS8638,Thank you.
Other Parts Discussed in Thread: ADS7841 , ADS7953 , ADS7953EVM-PDK , ADS8688EVM-PDK , ADS8684 , ADS8638 , ADS8638EVM-PDK , ADS7253 , ADS7254 How do i give the Din input to ADS7841 to start the ADC? I am basically testing the ADC chip in product engineering l…
Hi Kiran,
We have a number of devices in our portfolio that are still shipping after 20 years, so I don't have any reason to doubt that the ADS8634 and ADS8638 will still be shipping into 2023. There is a schematic for the ADS8368EVM-PDK in the back…
Part Number: ADS8638 Hi again,
I am using the ADS8638 in "manual" channel sequencing mode, i.e. I send SPI commands to the chip to manually select a particular ADC input channel. From my microcontroller, for testing I have a continuous loop which sends…
Part Number: ADS8638 Hi, I have noticed when using the ADS8638 that the first couple of reads of the ADC return "junk" data, after that it seems OK.
The command I am sending is 0x0810, which is a manual mode read for channel 1 (register address…