Other Parts Discussed in Thread: ADS8674 Hi,
I am using ADS8674IDBT in my design.
Please do let me know if it is compliant to REACH and ROHS. It would be great if you can provide any link for the same.
Regards,
Sandeep
Part Number: ADS8674 Hi team
My customer use ADS8674 in industrial PC, with x86 structure Linux system, the communication Interface is Intel GSPI.
Do we have the BIOS code for customer, is there any asi code for ACPI need to be added?
Thank you!
Jo…
Part Number: ADS8674 Hi, i have been testing this ADC to measure the analog input of a channel,
the issue is that when i send a MAN_Ch_n command to read the analog input channel 1 it pretty much always gives me the
same binary data. Even when there is…
Part Number: ADS8674
Hi,
Could you tell me about the power supply sequence? Which needs to be ramped first, analog power (AVDD and AVSS) or digital power (DVDD)? And what is the required ramping voltage?
Customer setup conditions: AIN=±15V, AVDD=5V, DVDD…
Part Number: ADS8674 Dear support team,
I communicate with the ADS8674 via a Raspberry Pi and the spidev package in Python and I am able to read the channels correctly.
E.g. for reading Channel 0 I send the 4 bytes [0xc0,0,0,0] and I receive the correct…
Part Number: ADS8674 Other Parts Discussed in Thread: ADS8678 Hey guys,
I am working with the ADS8678 EVM and appear to be having some issues with the communication. I have the board configured with default jumper settings and the GUI recognizes that…
Part Number: ADS8674 Other Parts Discussed in Thread: ADS8678 Hello E2E,
I Looking for EVM of ADS8674, I could not find it. Is it possible to evaluate ADS8674 on the ADS8678 EVM by implementing ADS8674? Is GUI saported for ADS8674? Regards, ACGUY
Part Number: ADS8674 Hi,
I used this component ADS8674 for a custom board ADS8674. Everything is in phase with our needs (number of channel=4, precision =14bits , SPI interface) except for cut off frequency of the component (15KHz see on datasheet despite…
Part Number: ADS8674 Other Parts Discussed in Thread: ADS8678 The SPI signals for an ADS8674/ADS8678 device are connected to GPIO lines on a processor and controlled through software to implement the SPI protocol for the device. After power on, the first…
Part Number: ADS8674 dear specialist;
my customer use ads8674 to design medical product, now they appear below phenomena, as below.
1.the chip can run normally firstly;
2. after running a period (about several days,may be three to five days,or more);the…