Part Number: AFE4403EVM Other Parts Discussed in Thread: AFE4403
Hello,
I have two thing to discuss:
1. I am using AFE4403 EVM, In the datasheet of AFE4403, it is mentioned that the output waveform is Inverted.
Can you make it clear that is it vertically…
Part Number: AFE4403EVM I'm using the AFE4403EVM along with the TI GUI to get PPG signal from my finger. For the Rx configuration, I use DAC cancellation current of 0.
I see a plausible signal in the LED1 and LED2 channels.
I expect to have small…
Part Number: AFE4403EVM Other Parts Discussed in Thread: AFE4403 , AFE4404 I understand from a previous post that the 3rd LED is "a static mode selection as opposed to dynamic switching selection. The device does not support simultaneous 3 LED operation…
Part Number: AFE4403EVM Is it possible to operate the AFE4403EVM Kit, set breakpoints in the firmware source, and check the association between the operation of the application and the operation of the firmware?
Hi, Since I did not hear back from you, I believe my suggestions answered your questions. I will close this post and if you have any pending questions, feel free to post them here or open a new thread. Thanks and have a great day!
Hi,
For Question#2 "my " TX_CTRL_SUP = LED_DRV_SUP = 4.9V". I am powering the EVM using USB port (J4) from the PC. Is this fine?"
" TX_CTRL_SUP = LED_DRV_SUP = 4.9V" are within the datasheet spec range.
"powering the EVM using…
Part Number: AFE4403EVM Other Parts Discussed in Thread: AFE4403 , Hello,
I am using AFE4403 EVM GUI, My GUI is working fine but when I try to launch the Macro window from the script option at the left upper corner of GUI interface it gives me this error…