Hi Fawn,
First we will need to check if the SPI is working fine. Can you enable the powerdown mode and check if the supply current is reduced? Since you do not have the data capture card TSW1400EVM, how do you verify the ADC data from the AFE5805EVM?
Hi Cesar,
Normally we do not release the Labview source code for the TSW1400EVM and the AFE5805EVM.
Can you provide your email address and we can take the conversation offline to discuss further?
Hi,
I am trying to interface AFE5805EVM to Zynq. Can you share me the code for deserializer? I have tried xapp524. I get the issue similar to one described in xilinx forum.
email : jothiadithya@gmail.com
Regards,
N Jothi
Yes I'm using AFE5805EVM RevB.
In DDR configuration the LCLK is 250MHz, but the ADCLK is 76,92MHz. (I want to use DDR mode)
In SDR configuration the LCLK is 500MHz, but the ADCLK is 80MHz.
So the problem is with with ADCLK frequency. Can I control…
Hi Chuck,
I'm working with AFE5805evm and TSW1400evm. Using HSDCPro if select device AFE5808 12b it works fine and I can see and save data.
I asked for this code, Jim Seton from High Speed Data Converter Forum send me a code but it is not working…
Hi Chuck,
No, Gui did not send me the code. Jim Seton sent me one but i think it is a AFE5809 code (because returns me the same error - frame clock not occurred)
No, I developed my own transmitter code that I can control beamforming, frequency, pulse…
Other Parts Discussed in Thread: AFE5805 , AFE5805EVM Hi,
I am designing a ultrasound device now. In AFE5805 datasheet, it says that the pin VCA_CS# (H4) can be connected to pin RST(H5). Does this means these two pins can be connected directly? In AFE5805E…
Other Parts Discussed in Thread: AFE5805 , AFE5805EVM I have got the TSW1250EVM_AFE5805 and AFE5805EVM.I want to modify the FPGA's program on TSW1250EVM.So I will be very appreciate if someone could provide me the suited source code of the FPGA on TSW1250EVM…