Part Number: AFE5807 Dear TI experts:
As regards to the AFE5807, i have some questions about the DNC pins, which are listed below. Could you kindly give me some help on this?
Thanks in advance!
Detailes of question:
Q1: what's insde the chip of the DNC…
Part Number: AFE5807 Other Parts Discussed in Thread: AFE5809 , SN74AUP1T04 Hi,
It seems there is no information in AFE5807 datasheet about output current (I_OH & I_OL) provided by the SDOUT pin. No info about the equivalent circuit for that pin too, so…
Part Number: AFE5807 Other Parts Discussed in Thread: AFE5808 , AFE5808A Hello,
My customer has a question about AFE5807 and AFE5808(A).
[Q]
Please tell me the difference between AFE5807 and AFE5808(A).
<My understanding>
* Analog Front-end : Sa…
Other Parts Discussed in Thread: AFE5807 hi
I am using afe5807, there are four adcs on my pcb board, when i set the TEST_PATTERN_MODES (ramp de-skew .....) , FPGA(XILINX V6) can aquire the correct data , but when TEST_PATTERN_MODES is Normal operation…
Other Parts Discussed in Thread: TX517 , AFE5809 , ADS52J90 , AFE5801EVM , AFE5801 , AFE58JD16 , AFE5816 , AFE5851 , ADS5294 , TX810
How to create an ultrasound system from TI’s ultrasound portfolio?
The signal chain would be TX517 -> transducer -> AFE58XX…
Other Parts Discussed in Thread: AFE5807 , AFE5808 , AFE5808A , AFE5809 Hi,
I would like to ask you a question about the difference between AFE5807/5808/5808A/5809.
Sorry, I do not understand well the major difference between these devices but noise performance…
Other Parts Discussed in Thread: AFE5807EVM Hi,
I am using a Zedboard evaluation kit along with FMC-DAC adapter and the AFE5807EVM from TI.
I would like to create a system that reads the LVDS output channels of the AFE5807EVM from the Zedboard FMC pins…
Hi,
The PGA clamp feature is not implemented in AFE5808. By default it is set at -2dBFS level. Setting bit 10 in 5808 will not introduce any undefined behavior. On a different note, there is a color noise issue in AFE5808 which was fixed in AFE5808A,…