Part Number: CC2652P
Not only SDK6.30 But also other SDK, this issue will happen in such condition. When coordinate and routers are transmiting busily, some of AF-Send with APS-Ack-Request-Enabled will not trigger "afDataConfirm". But the sending's record…
Part Number: CC2530 Other Parts Discussed in Thread: Z-STACK ,
My testing base on ZStack 3.0.2, end-device broadcast packets into air for long time. but on one occasion AF_DataRequest returns "Success" but AF_DATA_CONFIRM_CMD event was not triggered…
Hi Damon,
Damon Stewart said: The most recent AF_DataRequest() return status was SUCCESS. So the application is sending messages when it should, and the stack is responding with a SUCCESS status, even though they are never seen in the sniffer capture,…
Part Number: CC2530 Other Parts Discussed in Thread: Z-STACK , Z-STACK-ARCHIVE , Hello,
I want to send message between nodes without using ZCL. I went through some PDF guides and found the Af_DataRequest() API but i'm confused with its arguments especia…
Other Parts Discussed in Thread: TIDC-CC2530-CC2592EMK-RD , CC2592 hello all! I perform data transmission 1000byte / 1node. subdivided into 10 times of 50 bytes each, 50ms / 1 time. at a distance of 15-20m from the indoor. ZROUTER1 ------- ZC ---------- …
CHILD_RFD is a reduced function child device, which is as expected. You will see this in the Association Request's Capability Information (also including Rx On When Idle).
All queued packets to these devices will need to wait for a Data Request. The…
Hello Edan,
The Z-Stack solution involves higher-level API access to the IEEE PHY and thus basic RF commands cannot be used in this environment. I recommend using AF_DataRequest which you can understand more about in Z-Stack 3.0.2\Documents\Z-Stack 3.0 Developer…
Part Number: CC2538 Other Parts Discussed in Thread: Z-STACK Tool/software: TI-RTOS Hi,
About using AF_ACK_REQUEST in AF_DataRequest, I got confused. Please help to see which of my understanding below is correct (A or B)? If A, B are both wrong, please…
There is no single file for RF communication. You can review the Z-Stack 3.0.2\Documents\Z-Stack 3.0 Developer's Guide.pdf to further understand the ZCL, APS, BDB, NWK, and MAC layers. Typically a ZCL command will lead to AF_DataRequest which ultimately…
1.You can set up first parameter afAddrType_t *dstAddr in AF_DataRequest to use Addr64Bit but it's not recommended to do so.
2.You can use AF_DataRequest to send packet in proprietary format.