Part Number: BQ24060 I recently tested the BQ24060 battery charger with a battery pack that will be connected and removed frequently via a spring pin connector. Everything works great unless I remove the battery pack in such a way that the negative terminal…
Other Parts Discussed in Thread: BQ24060 , BQ25060 Hi Team,
My customer considers to use bq24060 or LTC4061 for 800mA charger in his application.
He thinks charge current accuracy of LTC4061 is higher than bq24060 as following.
------------------------…
Other Parts Discussed in Thread: BQ24060 Hi TI,
In my current design (schematic proprietary unless shared under NDA), I'm using the bq24314cdsgt as a front-end protection chip for my LiPo charger, which is also one of yours (bq24060) .
Anyway, despite…
Other Parts Discussed in Thread: BQ24060 , BQ24032A , BQ24050 Hi Team
I looking for LiIon 1 cell charger with LDO including.
We found several Charger LDO internal type, For instance BQ24032A, BQ24060, BQ24050.
I have some simple question for some device…
I have similar problem with BQ24060. It reduce the current down to 20 mA and it also reduce voltage output to 1,8V. When I have a LiPo battery with protection circuitry it will not take any current before voltage rise to 3V. Is there any trick to get…
I do not recommend that unless you can accurately predict the amount of voltage drop due to resistive losses and slowly scale back the regulation voltage so that you do not overcharge the battery.
One of our older non-power path devices (bq24060) has a…
Other Parts Discussed in Thread: BQ24060 Hi there,
I'm a newbie to electronics. I'm looking at getting a pcb made up which will require a charger for a 2000mAh lipo battery. I saw the bq24060/64 (shown below), but i'm not sure if it is suitable…
Other Parts Discussed in Thread: BQ24072 , BQ24031 , BQ24079 , BQ24060 I am looking for an IC that can do active power management ( most important function is load switch from the battery to the external supply ), and can allow a battery charge rate of 50mA…
Other Parts Discussed in Thread: BQ24060 , BQ24079T , BQ24079 Dear Friends,
I am very new to battery charging technology. I am working on project which demand battery charging. I want to charge 3.7v , 1200 mAh lithium ion battery. I want over charging…