Part Number: BQ24171 Hi
The customer design with BQ24171 to charge the 2 cells. They follow the datasheet 9.3.15 to do the battery detect test.
It was found that at the beginning of charging, charging stopped after maintaining a 100mA charging current…
Part Number: BQ24171 Hi Team,
The customer uses 2 string batteries. The battery voltage is set to 8.4V. Before charging was terminated, the battery voltage was measured to be around 8.38V, but after charging was terminated, the battery was not actually…
Hi Germain,
Thank you for the feedback regarding the different charger ICs proposed.
Please let us know if you have any additional questions.
Best Regards,
Garrett
Part Number: BQ24171 I have some queries related to the design of the BQ24171 charger circuit.
Q1. In the application circuit of the same, a N channel reverse blocking FET is added in the circuit ,whose source pin is connected to the source of ACFET.…
Part Number: BQ24171 Other Parts Discussed in Thread: BQ24172 Hi,
We are using BQ24171 charger IC in our board and 103AT NTC thermistor. We want to set charging temperature T1 = 0ºC for COLD and T5 = 45ºC for HOT. Please tell me calculated RT1…
Hello Akilarasan,
No, to configure the gauge you will need BQStudio to upload the ChemID onto the gauge since it contains proprietary information.
Regards,
Jonny.
Part Number: BQ24171 Other Parts Discussed in Thread: BQ25616 , BQ25606 Hi, T.I's FAE, hello!
The following picture is the schematic diagram I designed for BQ24171. Could you please help review if it is correct? Thank you.
Among them, my power input…
Part Number: BQ24171
Hello, FAE of Texas Instruments
I have some debugging issues with BQ24171 that I would like to consult with
Q1: At the beginning of debugging, there was no output because I set the PGND and AGND corresponding to the typical application…
Part Number: BQ24171 Hi Jeff
I have a few questions about device parameters that I would like to ask you
Attached is my schematic diagram
Q1:Can I use 4.3K for R105&R106 in the schematic diagram?
Q2:Is it correct for me to use 5.1 Ω for R112 in the…
Part Number: BQ24171 Hi
I have a query need your help.
If I do not need the power path, t he SYSTEM voltage is equal to the battery voltage, does the battery voltage pass through BQ24171?
Waiting for your reply.
Thanks
Star