Hi Jeff
Thank you for advice,
Customer information is update; When 5V bus add to connect 1Ω for avoid overvoltage, EN toggle was normal operation.
But waveform occur ringing and IR drop affect to add 1Ωresistor.
・500mA condition (EN2: 0…
Other Parts Discussed in Thread: BQ24251EVM-150 Hello,
does BQ24251EVM-150 include also the adapter that enables the EVM to be connected to PC or do we need to buy it separately? Is that adapter called USB-TO-GPIO?
Part Number: BQ24253 Other Parts Discussed in Thread: BQ24251EVM-150 , BQ24250C Hi Team,
I would like to evaluate charger + fuel gauge from TI .
In my application I looking for charger with D+/D- so I found BQ24253.
I found that TI doesn't have EVM for…
Other Parts Discussed in Thread: BQ24251 , BQ24251EVM-150 Hello~
I need your help for battery charger.
Below is my schematic of BQ24251 and is using the QFN package.
NTC is not using and rest of resistors are 20K & 20K such as bq24251EVM-150.
Test procedures…