Part Number: BQ24610 Hello,
The charging of BQ24610 is normal, but the status indicator light is not working properly. There are three indicator lights: power indicator light, charging indicator light, and charging complete indicator light. The current…
Part Number: BQ24610 Hi
The customer design with BQ24610, when the battery is not connected, ISET1 and ISET2 waveforms are found to be abnormal, as shown in Figures 1 and 2.
When the battery is connected, the output battery voltage is abnormal in figure…
Part Number: BQ24610 Good morning, following the guide in the bq24610 datasheet, I arrived at this circuit with these values. Regardless of whether the configurations are correct or not, I calculated a VBAT of 11.1 because I will be using 3 batteries…
Part Number: BQ24610 Hi
The customer design with BQ24610, the PCBA made by EVM Gerber used on the official website. During the test we found that both HIDRV and LODRV have waveforms, but the battery cannot be charged.
Attached the schematic
CH2: Q3 Gate…
Part Number: BQ24610 Hi
The customer design with BQ24610.
The HIDRV and LODRV output have failed in charge process, normal is PWM waveform, failed waveform is p ulses with a period of 4ms, the STAT1 STAT2 PG is normal voltage.
HIDRV output
BTST volta…
Part Number: BQ24610 Hello,
The charging of BQ24610 is normal, but the status indicator light is not working properly. There are three indicator lights: power indicator light, charging indicator light, and charging complete indicator light. The current…
Part Number: BQ24610
Hi
Is there any risk if I use a 24V adapter to hot-swap the BQ24610 directly? If BQ246102 can support 24V hot swapping, many parameters need to be confirmed.
Even if I change a adapter, I need to re-confirm and test it repeatedly…
Part Number: BQ24610 Hello,
I'm trying to create a 12V lead-acid battery charger based on BQ24610:
The battery I'm using is quite small, only 0.8Ah
sense resistor 50mohm
the charging current is set to 300mA
termination current 50mA
Charge voltage…
Part Number: BQ24610
Hi All!
Please take a look at my particular problem with weird behaviour of my circuit.
I have a 6 cell Li-ion package. My target charging voltage is set to 24.66V (with VFB pin), fast charge current set to 1.06A (with ISET1) and…