Part Number: BQ25713B Other Parts Discussed in Thread: BQ25713 Tool/software: Hi,
My name is Antonio López and I have a few questions about the BQ25713B:
Which is the difference between BQ25713 and BQ25713B?
Can I make my own PCB with the typical…
Hi Tim,
Both of the them are the same chip except that the I2C addresses are different. BQ25713 has address 6Bh while BQ25713B has address 6Ah for I2C communication.
And yes they are interchangeable.
Best Regards,
Munir
Part Number: BQ25713B Other Parts Discussed in Thread: BQ25730 , BQ25731 Hi,
Our design uses a BQ25713B with an adapter input voltage of 24Volts. In PTM mode both highside switches are open and the 24V are passed through to VSYS.
The datasheet states an…
Part Number: BQ25713B Other Parts Discussed in Thread: TPS25750 , , BQ25713 Dear Suppot Team,
we are currently debugging a board with the combination of TPS25750 and the BQ25713B. In my understanding the TPS25750 supporting only the BQ25713 (without the…
Part Number: TPS25750 Other Parts Discussed in Thread: BQ25713B , BQ25713 , BQ25790 , BQ25731 The main board of our product uses TPS25750 and BQ25713B as the power management solution.
When we used the Application Customization Tool to configure the PD controller…
Part Number: BQ25713B Other Parts Discussed in Thread: BQ25713 Hi,
My customer wants to know if they can config the BQ device for re-activation of the over discharge battery.
When the battery is over discharged(0V), it will need 6.6V to reactivate. Right…
Part Number: BQ25713B Other Parts Discussed in Thread: BQ25713 Hi
I have a query need your help.
When I remove the adapter, r egisters cannot be read and written when in boost mode. Does it normal?
The register setting as below:
struct bq257xx_reg_st bq25…