My application is to develop a wire-less charging ckt for IoT based system(This much info I can provide)
Please clarify me below details:
1.Whether suggested transmitter complies with the both BQ51051BRHLR& BQ51013.
2.Is BQ50002AEVM-607 is same as…
Hello Gianluca
The bq500210EVM-689 is our 19V input TX, WPC TX type A1 or A10. The coil should have an inductance in the range of 24uH. Also low DCR is desirable.
TX is a resonant converter topology and even with no load on the RX the circulating current…
Part Number: BQ51025 Other Parts Discussed in Thread: BQ500210 , Reference case # CS1183495.
Good evening. We recently acquired the BQ51025EVM-649 wireless receiver module to replace an older model (BQ51013EVM-725) that we use for testing. We use the receiver…
Because of an unexpected power-off,the 3V3_VCC and the GND short circuit.on the bq500210EVM-689 ,the voltage on TP10 are 0.4V when power on.I want to know what's the most possible reason and how to repair the circuit. Besides,I want to know some data…
Other Parts Discussed in Thread: BQ500210 Hello
I'm studying about wireless power and practicing on this board: BQ500210EVM-689.
I found on the internet, but i don't find anything relate to source code examples as well as firmware for
this board…
Hello~
If possible, would you please let me know the MLCC manufacturer name for C7, C13, C15, C27 which are used to bq500210EVM-689 TX EVM?
According to BOM list of bq500210EVM-689 TX EVM user's guide, I just find "STD" at part number as well as manufacturer…
Hello~
According to "bqTESLA FAQ", there are the WPC Certification numbers for some TX and RX EVM modules...
But, there is not WPC Certification number for bq500210EVM-689 TX EVM module...
If it does not matter, would you please let me know…
Part Number: BQ51013B Hi,
I would test wireless power transmission. I have the power transmitter evm BQ500210EVM-689 that is WPC 1.0 compliant. Can I use BQ51013BEVM-764 (that is WPC 1.1 compliant) as receiver?
Best Regards
Fabrizio
Anj,
The 10V capacitors will most likely be damaged in the system. If they are not damaged, the capacitance values will be very low compared to their stated values. In either case, long term use will not provide satisfactory results.
The bq500210EVM-689…
Other Parts Discussed in Thread: BQ51013 , BQ500210 , TIDA-00762 I am currently using BQ500210EVM -689 (760308101 coil) and designing the different receivers with your coils. I am using bq51013 and bq51050 Texas instruments chips. I tested 760308201 and…