Hi George,
Sorry about that. BTW: This compiles OK on version 18.1.8 for the F28379D, but fails on the F280049.
John
**** Build of configuration Debug for project GEN3HandHeld ****
"C:\\ti\\ccsv8\\utils\\bin\\gmake" -k -j 16 SerialQueue.obj -O…
Mark,
Please refer to pg. 32 for Bob Pease's comment on LM335. He basically said that 0.1uF+22ohm is fine. The article also pointed out a way to validate the stability empirically if you're interested in other cap values.
Bob Pease Lab Notes Part…
Hi Dominik,
SOC starts to the drop at 7% when discharge.
How can I adjust it?
Attached are the log data and gg file.
25degC 500mA dsg(0713).csv Draft gg V00 (0715).gg.csv
Please help me confirm.
Thanks!
Regards,
Peter
Hi Subhajit,
In earlier mail chains I have attached output of ls -lR targetfs/ .
and have followed steps mentioned in VisionSDK_LinuxUserGuide document for linux installation on A15.
and I dont find any source code after installing omap5-sgx-ddk…
>> The ptp announce packet loops (sent every 5-30 microseconds).
Here are the logs when looping announce and sync packages. logs_pcap (2).txt
Regards,
Dimitry
Hi Garrett,
How much time (minutes, hours) does the connection get dropped?
About one minute.
It can auto-recover without any intervention.
This is the log from PLC.
This is the error frame from Wireshark.
Attached is the whole…
Hi Bob,
i tried with 29 bit Identifier with 0x7DF ID and mask is 0x1FFFFFFF value. i am able to receive a data but i can't able to question to frematics. Previously with 11bit Identifier, i got a results.
My settings are
so by using this settings…
Part Number: TPS546D24A Hi,
Please verify the attached layout for TPS546D24ARVFR, Vin - 12v, Vout - 0.85V. Schematics and design calculator is also attached for reference.
Thanks
/cfs-file/__key/communityserver-discussions-components-files/196/TPS546D24ARVFR_5F00_1…
Hi Ricky,
The *.DWI file was attached. It seems like some dll files are missing. Please take a look at the attached file. Would you mind to let me know how to solve this issue? Thank you.
PS:Please change the extension file name from .txt to *.dwi…