Part Number: CC1312R Tool/software: Hi,
I wanted to use this microcontroller to control the 6 electric actuator mounted inside locomotive & controlled wirelessly using a web page from a control room, I want to know the wireless range of the device, need…
Part Number: CC1312R Other Parts Discussed in Thread: CC1310 Tool/software: What is the balanced low-import impedance of pins 1 (RF_P) and 2 (RF_N) of the CC1312R1F3RGZ?
Part Number: CC1312R Tool/software: I am using CC1312R to develop products using 920MHz and 1200MHz frequencies.
However, the overall noise floor at 920 MHz is high and spurious around the carrier wave does not meet the standard.
The 1200 MHz band also…
Part Number: CC1312R Tool/software: Hi
I am designing a transmitter circuit using CC1312.
We are considering a circuit that satisfies the following frequencies in one circuit. 300MHz band, 400MHz band, 900MHz band and 1200MHz bands.
I am thinking of ways…
Part Number: CC1312R Other Parts Discussed in Thread: CC1312PSIP Tool/software: I need FCC approval for several products using the CC1312R MCU.
However I can not seem to locate a FCC ID for a modular FCC grant in the datasheet, I can only find a note…
Part Number: CC1312R Tool/software:
We see an issue with the UART2-driver that leads to a lock-up of the driver.
The UART is configured as UART2_Mode_CALLBACK in both read and write. We use simplelink version 7.10.01.24
If we very frequently send data…
Part Number: CC1312R
Tool/software:
I do not seem to get UART 1 working. Please help me understand what I have done wrong. I am using the rfUARTBridge_CC1312R1_LAUNCHXL_nortos_gcc example to test my code out. I have run syscfg, and added a uart, it uses…
Part Number: CC1312R Other Parts Discussed in Thread: CC1310 , UNIFLASH , Tool/software: Hello,
I am getting a programming error trying to program a basic CC1312 board. I am using a CC1312R1 Launch XL to program and am getting the follwing error. Forced…
Part Number: CC1312R Other Parts Discussed in Thread: SYSCONFIG Tool/software: Sorry to ask, perhaps obvious to some...
I try to add a SPI device to my CC1312 board in making. I get the suggestion to use the following pins
SCLK 16/32
POCI 15/11
PICO 12…
Part Number: CC1312R Tool/software:
Hi team,
My customer is using CC1312R to do RF certification at RF lab. They have some questions while following FCC Part15C for Sub1GHz :
www.ecfr.gov/.../section-15.247
Question 1 : Which mode should be chosen…