Part Number: CC2500 Tool/software: How much jitter does CC2500's bit synchronization algorithm have?
Used under the conditions of data rate 250kbps and modulation method FSK.
Part Number: CC2400 Other Parts Discussed in Thread: CC2500 , Tool/software: The CC2400 and CC2500 have RF differential outputs. When designing a balun for these ICs, it is necessary to set the component constants considering the characteristics of the…
Part Number: CC2500 I have followed the reference design for the CC2500 balun and pie network to match to a 50 Ohm antenna.
What are the expected losses through these external circuit components ?
After some tuning and improving I see about 11dBm loss…
Hello Kien Nguyen,
I did a text compare between the CC2500 whitening mode and the PN9 mode we get the following differences (PN9 is the red, CC2500 mode is green):
in the rf configs .c file we get
in the rf configs .h file we get
So one register is…
Part Number: CC2652P Other Parts Discussed in Thread: CC2500 Hello,
I want to make a wireless connectivity between CC2652 and CC2500. Is it possible? Can someone share the required configurations for both?
Part Number: CC2500
Hello everyone. We are using a single CC2500 on a custom board for the transmission and reception of data.
Our intention is to configure the chip with MSK modulation at 2425 MHz. We aim to operate at a 1 kbps data rate with FEC…
Part Number: CC2500 Hi,
We received an inquiry from one of our customers. I can't find an answer from D/S, so please let me know.
1. Regarding sine wave input, it is described as "peak-to-peak amplitude of up to 1V." What is the minimum peak-to-peak…
Part Number: CC2500
Hi team,
The customer said:
Due to the deviation of PCBA components, the final communication frequency will be deviation. Does CC2500 have a mechanism to calibrate the communication frequency?
Is calibration achieved by sending the…
Part Number: CC2500 Hi Team,
I have a machine here using the CC2500 module that can receive normally at first, but cannot receive after a while.
I switch the mode to transmit, and the module can work normally, but it just cannot receive, and the software…