Part Number: CC2531 Tool/software: Since I never heard back about using an external oscillator, I have switched back to using a 32MHz crystal tied to pins 22 & 23 with loading caps. When powered, the chip always enumerates with my laptop (windows…
Part Number: CC2531 Other Parts Discussed in Thread: Z-STACK , CC2652P , CC1350 Hi, i'm trying to build some java code to backup the dongle CC2531, in particular the state of the network. If a lose the key or it breaks, I want to restore it without making…
Part Number: CC2531 I am using the CC2531 with an external 32MHz oscillator connected to to XOSC_Q1 (pin 22). Do I need to anything with XOSC_Q2 (pin 23)? For example, I know that some chips require grounding the other clock pin when using an external…
Other Parts Discussed in Thread: CC2531 , CC-DEBUGGER
I am facing an issue for flashing the CC2531 Dongle as ZigBee concentrator. My CC debugger is not able to detect in flash programmer.
Please help me on this part.
Also provide the steps for making…
Part Number: CC2531 Other Parts Discussed in Thread: CC-DEBUGGER Hi,
My Ubiqua Protocol Analyzer is not detecting the CC2531 packet sniffer. Please let me know how to fix this
Thanks,
Rajesh Krishnan
Part Number: CC2531 Hi,
When I use SmartRF Studio Expert Mode (Packet RX) I get less packets than SmartRF Packet Sniffer, Why is that?
Can I use SmartRF Packet Sniffer to capture non-standard zigbee frequencies like in SmartRF Studio Expert Mode?
Thanks…
Part Number: CC2531 Other Parts Discussed in Thread: CC2530 , Z-STACK
Hi Experts,
I need your assistance here to find the right device for our customer.
Regarding this CC2531 Dongle, they usually use it with the packet sniffer software to get the…
Part Number: CC2531 Other Parts Discussed in Thread: , PACKET-SNIFFER Hello everyone.
It is not my habit to be posting on forums but I've been stuck on the problem for days.
I have two CC2531EMK dongles that I am using for Zigbee testing. Both are…
Part Number: CC2531 Hi Experts,
Our customer has a question about the CC2531.
If the USB module is not currently being used, can the VUSB be left Open or must it be tied to +3.3V?
Also, if Vusb does not have to be tied to +3.3, should it be pulled down…
Part Number: CC2531 Hi,
Iam try to control the loads via ztool using 4 load switch when i control the single load but other load are turns on. i check the AF data Request command single load is sended.
Start Time: 12/17/2022 3:12:14 PM
<TX>03:13:35.27…