Part Number: CD4017B Tool/software: 07cs31ke4 CD4017BE: Trying to use this Decade Counter as a channel gate control device, However after connecting the device by the approved schematic, the device does not Sequence through outputs and only stays on Q0…
Part Number: CD4017B Other Parts Discussed in Thread: CD4514B , CD4510B , SN74HCS74 , SN74HCS164 Hi Experts,
Our customer is looking for a schematic for the CD4017B cascade timer for 20 to 80 lights. He have a few circuits he got off the internet…
Part Number: CD4017B Dear Sir/ Madam,
If we supply 3.3V to CD4017B, what is the threshold for input high and low voltage(VIL, VIH)?
Datasheet provide data for 5,10,15V supply but no 3.3V data.
I just want to confirm if it is 70% supply voltage…
Part Number: CD4017B Dear Sir/Madam,
I just look into CD4017B datasheet, supply voltage range should be 3-18V, but datasheet provide 5V, 10V and 15V data only.
Can i implement it on 3.3V circuit? and 3.3V as logic high level?
Thanks.
Best…
Thomas,
There is always a way to make the model and it would be in the form of a custom spice macro. You could use the schematic in the datasheet and some basic gates to create a decade counter or you could try to find an existing PSpice decade counter…
Other Parts Discussed in Thread: CD4017B Hi
Where can I get a spice model for CD4017B?
I have a pspice model but produces error:
"Not supported syntax element LOGICEXP"
Thanks
Hi Chad,
Thanks for the response. I have not tried that suggestion but it's a good idea.
The device does work at f<1k, just not reliably. My 2 hour timer lasted about 2.2 hours, so I thought using an external oscillator would be a good solution. …
Kiryl,
The time periods can be ratios, such as all steps are the same width (1:1) If the ratios can fit into 10 time steps or less then CD4017B can team up with a single NE555. The NE555 sets the repetition rate (output frequency). The CD4017B sets…
Hello chennangan,
For a square wave of such low frequency, unless you need extremely low jitter, it makes the most sense to use a microcontroller to directly sample the square wave at much higher frequency and program the microcontroller as a digital…