Part Number: CD54HC4046A Tool/software: Hello,
I'm planning to use this
CD54HC4046A chip for FSK demodulation. Can it demodulate 380 KHz to 480 KHz data rate FSK?
Please advice.
Thank you,
Muthu
Other Parts Discussed in Thread: CD54HC4046A , SN74LVC1G58 Hi Guys,
I am planning to design an sensor module for HF ATU (3MHz-30MHz).
The input to me will be coupled forward PWR signal and Reflected PWR signal.
I have to give phase difference between…
Hi Fabrice,
Maybe you can check if the HC series has better precision, they are the high-speed version pin-compatible version of 4046B.
https://www.ti.com/product/CD54HC4046A
CDCE813-Q1 is Q100 qualified, but the CD74HC4046A is not. However, I noticed that CD74HC4046A has a temperature range from -55 to 125. I am not an expert on CD74HC4046A, this device is supported by another team. I noticed that there are some military…
Mathieu,
The LMK4100 series can handle the 1 kHz input frequency and generate your output frequency, but is much higher than 5 mA.
We have LMX series PLLs that are below 5 mA (LMX2430), but can't handle 1 kHz input or go down to 16 MHz. I couldn't…
He Dean,
My input is a swept sinusoidal, the LMX2485 or LMX2430 frequency is too high. My input frequency is max 100MHz. I have looked at the CD54HC4046A and in the datasheet there used a square as reference input signal. Is it’s possible to used swept…
Other Parts Discussed in Thread: CD4046B I know that the vco for the cd4046b only goes up to 1.4 MHz but I need to use its xor Phase Detector and input amplifier at 13.56 MHz. Will this device work at this frequency?
Other Parts Discussed in Thread: CD74HC4046A I'm trying to use the CD74HC4046A PLL w/VCO chip to set up a low-frequency PLL circuit. I'm observing odd behavior and am having a hard time understanding what is going on with the chip. I am using phase comparator…