Part Number: DAC80004EVM Tool/software: Hello, In ESP8266 I have my MISO MOSI CLK and chip select. Where do i connect them in the EVM board? The teminology is not the same so i am not sure where exactly to connect it?
Thanks. https://www.ti.com/lit/ug…
Part Number: DAC80004EVM Other Parts Discussed in Thread: DAC80004 , DXP , Team,
Can you please clarify what option are available to evaluate the DAC80004. See below questions:
a)Apparently the DXP SW (that was originally used for DAC EVM eval) can only be…
Part Number: DAC80004EVM Other Parts Discussed in Thread: DAC80004
Hello, I have bought DAC80004EVM shown bellow.
I want to program it using Jlink debugger with pin out shown bellow in the poto bellow on the left. Where do connect the Jlink pins on the…
Part Number: DAC80004EVM Other Parts Discussed in Thread: DAC80004 Hi Team,
My customer will design DAC80004 in PLC AO project and got a EVM on hand. Customer is asking for SPI sample code then FW engineer will test EVM performance with their MCU board…
Part Number: DAC80004EVM Other Parts Discussed in Thread: DXP , ADCPRO Hi,
My customer was wondering if we had any sample code available for the DAC80004EVM that showed using the SPI features with full duplex for sending commands and querying the status…
Part Number: DAC80004EVM Other Parts Discussed in Thread: DXP Got the DAC80004EVM. If I correct its required also the MMBO board too.
Is it correct?
How to order it?
The related s/w tool is the DXP DAC Exerciser Program?
Part Number: DAC80004EVM Other Parts Discussed in Thread: DAC80004 , DXP Hi all,
As DAC80004EVM requires TI Modular EVM Motherboard MMB0, I currently get one for revision C.
I wonder if DAC80004EVM compatible with MMB Rev.C.
Part Number: DAC80004EVM I can write to the DAC to change voltages but have not been able to read back the data/status. Any Ideas?
Sent: (With sync high between every 32 bit xfer.)
0x07 0x00 0x00 0x00 - Reset DAC
0x08 0x00 0x00 0x02 - Enable SDO
0x1D…
Hi,
These digital interface pins are connected to J2B in the schematics as shown below (marked with green color box). This DAC80004EVM board can be used as a standalone board or as a daughter card to the MMB0 Modular EVM motherboard. The MMB0 motherboard…
Hello, I have made a more clear photos when i sent only the first command
{0x03,0x0F,0xFF,0xF0} 1.am i supposed to see VDD on channel 0?
2.from the photos shown bellow,do you still say i have a clock problem?I will try the same SPI sequence on The DAC80004EVM…