Part Number: DAC8760 Other Parts Discussed in Thread: OPA192 , , , TIPD119 Hi, I have some questions, could you please help me? 1. Unused HART-IN Do I have to tie HART-IN pin to GND through a 22 nF capacitor or can I leave it floating? 2. Does the DAC only…
Part Number: DAC8760 Hi support team.
I have two questions regarding TUE (total unajusted error).
1. Is the formula for calculating TUE as follows? Also, are the calculations given in the example correct?
TUE=sqrt(GE^2+OE^2+INL^2) GE:gain error OE:offset…
Part Number: DAC8760 Hi support team all.
This is a question from my customer.
Are offset and gain errors checked during shipping testing?
Also, do you make any corrections if the error exceeds the specified limit?
Best regards,
Higa
Part Number: DAC8760
Hi team,
When my customer used DAC8760 in PLC AO module, it seems the output ramps up very slowly in micro seconds. The external circuit is shown above. Do you have any idea how this happened? What should be modified based on external…
Part Number: DAC8760 While reviewing the DAC8760 datasheet, I noticed that there is a power-up procedure.
It is specified that AVDD power must be supplied first and DVDD power must be supplied later. How does the DAC8760 operate if the conditions are…
Part Number: DAC8760 Hi team,
I would like to ask if we reset by setting the DB0 bit, if any delay time we need to wait or it will work immediately ?
I didn't find instructions for this in the datasheet. Could you help check this?
Thanks
Lillia…
Part Number: DAC8760 Other Parts Discussed in Thread: DAC8771
Hello guys,
One of my customers uses DAC8760 for 4mA-20mA interface of their current mass-productions.
At this moment, they have the following question. Could you please give me your reply…
Part Number: DAC8760
After implementing CRC in all our devices utilizing eight DAC8760 units in a daisy chain configuration, we continue to experience long-term stability issues. It appears that our daisy chain intermittently "breaks" at unpredictable…