Part Number: DLPC3470 Tool/software: Hello,
Recently started working on the EVM mentioned in the title. Had got a driver installer that contained the Cypress USB adapter.
I recently updated the firmware on the board using the latest firmware from TI…
Part Number: DLP2010EVM-LC Hi,
I'd like to know if it is possible to display custom generated images in real time with the DLP2010EVM, using the DLPC API with USB connection only, without using the HDMI channel (we can only connect the USB cable).…
Part Number: DLPC3470 Other Parts Discussed in Thread: DLP3010LC , DLPC3478 , DLP3010EVM-LC , DLP2010 , DLP2010LC
Hi,
We are currently developing DLPC3470 custom display board while checking the reference design for the evaluation board DLP2010EVM-LC.
While…
Part Number: DLP2010EVM-LC
Hello Ti Community,
i have a problem with my DLP2010EVM-LC. Let's me explain.
I worked with the DLP during 4months and it worked well.
I broke the flex cable. So i bought a new one with EKBtechnologies.
But now, i can"t…
Miguel,
In order to re-flash the firmware, please toggle the SW on/off switch to off position (The GUI now should indicate "Connected, Powered off") and the re-program the firmware available on the EVM page ( https://www.ti.com/tool/DLP2010EVM…
Part Number: DLP2010EVM-LC
Hi Team, seeking your assistance.
Broken Zemax/OpticsStudio file for the DLP2010EVM-LC optical setup. The file seems to be broken in two ways:
Two out of the three configurations do not work.
The field of view specified in…
Part Number: DLP2010EVM-LC Hello Guys,
Good day.
Our customer is using 2 DLP2010EVM-LC with their own DMD chip. He can operate only one of them at a time from the DLP EVM GUI. Is there a way to connect both modules and operate them simultaneously? Should…
Part Number: DLP2010EVM-LC When I use my industrial camera to directly shoot the DLP2010EVM-LC and I use hdmi to connect my computer to the DLP2010EVM-LC, when I give a fixed color picture, why my industrial camera's preview picture gives a periodic flickering…
Part Number: DLP2010EVM-LC Hello TI Experts,
I have a question about the DLP2010EVM-LC GUI.
I connected the DLP2010EVM-LC GUI with PC and tried to connect from the GUI tool.
But if I tried to push Get button to get the EVM information, the message like…