Part Number: DLP3000-C300REF Hello,
I'm currently using a DMD DLP3000 and it is not connecting to the GUI sofware. I've tried many things already. First I tried installing it to a Windows 7 computer, following the instructions from the manual (Installing…
Part Number: DLP3000 Hi,
I have a DLP LightCrafter 0.3 WVGA chipset with DPL3000, I would install the graphical user interface but the only available version corresponds at DPL3010EVM, the problem is that after plugging the DLP and connected the USB…
Thanks a lot, Hirak. That sounds promising to us. We will probably switch back to DLP3000. One more question, does this reset signal (for DLP3000) only occur when we change the pattern?
Part Number: DLP3000 Hi ,
I am using DLP3000 lightcrafter kit.
I am using the 3D scanner executable program named 'DLP_LightCrafter_3D_Scan_Application.exe' .
The scanning works fine after calibration.
Is there any way of saving my current calibration…
Part Number: DLP3000-C300REF I am presently using a DLP3000 LightCrafter EVM without the Light Engine(removed after buying since I use the mirror array directly with a laser and has been working well for several years) which upon connecting to the power…
Part Number: DLP3000-C300REF Dear Staff;
I have one question about model DLP 3000.
What is rotate angle of DLP 3000? I saw the rotate angle of DLP 3000 at manual and some people's FAQ.
In the manual of DLP 3000, the rotated angle is (+/-)12 degrees…
Part Number: DLP3000 How do I perform factory reset of DLP3000?
What are the compatibility versions for DM365, FPGA and MSP430? our DM365 version is showing 3.31 but I couldn't load any FPGA and MSP430 versions in the system???
How we can download…
Part Number: DLP3000 Hello i have the dlp3000 lightcrafter and i need to know, in the light engine what types of rectangular (possibly dichroic) mirrors and led focus lenses are used...?
Part Number: DLP3000 Hello,
I've used Jan Winter's MATLAB code to connect to the DLP3000. While I can establish a connection to the DLP, I cannot create any changes to the mirror configuration on the device.
I tried running:
L=LightCrafter()
…
Part Number: DLP3000 Hello,
set DLP3000 ethernet settings as fixed IP (192.168.1.99) as shown below. But there are other network connections on the same computer (wireless/wired). But they might be in conflict in some cases especially in Win 10. That is…