Part Number: DLP6500FYE Other Parts Discussed in Thread: DLPC900 , DLPLCR65EVM , , DLPLCRC900EVM I'm trying to follow instructions on setting up my DMD and evaluation board on Lightcrafter software. I have the issue that on the operating mode, I can't leave…
Part Number: DLP6500FYE Other Parts Discussed in Thread: DLP6500FLQ , DLPLCR65FLQEVM , DLPLCRC910EVM , DLPLCR65EVM , DLPLCRC900EVM , DLPC900 , DLPC910 Hi,
I want to buy the EVM systems about DLP6500 series for laser patterning, aiming for a high power output…
Part Number: DLP6500FYE Other Parts Discussed in Thread: DLP7000 I intend to use a TIR prism I would like to use a DLP6500 or DLP7000, but they must be illuminated from a position perpendicular to the micromirror hinge axis, i.e. 45°, and at an angle of…
Part Number: DLP6500FYE Hello, I would like to ask a question. I built a projector system with DLP6500: a laser shoots on the DMD chip with an elevation angle of 24° and an azimuth angle of 45°. The pattern will be projected directly above the DMD…
Part Number: DLP6500FYE Other Parts Discussed in Thread: DLPC900 How to safely cut off the power and disconnect the DMD chip and its controller with computer? Thx
Part Number: DLP6500FYE Other Parts Discussed in Thread: DLPC900
As the picture shows, when the display is stoped (pattern on the fly mode), there still a fringe display on the DMD, Thx. When a group of pictures are loaded to display, the same fringe…
Part Number: DLP6500FYE When the output light from the laser diode is collimated and irradiated to the DMD, several images of reflected light from the DMD appear to overlap. What could be the cause of this? I am using a DLP6500FYE Thank you.
Hello again Paul,
A command log would indeed be very helpful for the software team. Thank you.
I am confused about these two statements:
Paul Ross said: my driver is part of a single threaded loop that can only execute one command at a time, and thus the…
Part Number: DLP6500FYE Other Parts Discussed in Thread: DLPC900 Hi,
I am currently using a DLP6500FYE connected to the DLP Lightcrafter DLPC900 Evaluation Module. I would like to be able to precisely control the exact refresh rate of the DMD, the hope…