Part Number: DRV8306 Other Parts Discussed in Thread: DRV8320 , DRV8328 , DRV8323 , DRV8329 Hello Team,
we have already developed BLDC driver using DRV8306 for normal linear operation. we want to upgrade the design by including below features in it.
1.…
Part Number: DRV8306
Hi, experts.
I am encountering issues with the Motor Driver DRV8306 and Ti Mosfet CSD88584.
I chose this mosfet after observing it on TI's EVM Board, which utilized the DRV8306 and CSD88584 Mosfet.
My system comprises an ST microcontroller…
Part Number: DRV8306 Not sure what the issues is but when I apply power. I don't get the 3.3 VDC out to run the hall cells.
DRV8306-S.pdf
DRV8306-BT.pdf
Part Number: DRV8306 Hi,
In regard to the previous question, it was explain how to select the R_ISEN value (Based on the 0.25 Vlimit).
From that I derive that the power rating of the resistor should be I_max^2*R_ISEN.
If I look at the selected R_ISEN…
Part Number: DRV8306 Other Parts Discussed in Thread: CSD18514Q5A , CSD88584Q5DC Hi,
I would like to understand how to calculate R_ISEN?
In the EVM it is set to 0.007Ohm but I do not know the pulse by pulse current limit based on it.
From what I can understand…
Part Number: DRV8306 Other Parts Discussed in Thread: DRV832X , DRV8350 , DRV8323 , DRV8353 , DRV8320 , MCT8316Z , MCT8315Z Hi everyone,
We are using DRV8306 to develop a custom motor controller. During no-load spinning of the motor the controller works good…
Part Number: DRV8306 Hi Experts,
I am designing a new motor driver based on the DRB8306.
I read the data sheet and the EVM guid and have some questions.
1. Bellow is the section from the data sheet with the respected VDS_OCP values:
In section 8 there…
Part Number: DRV8306 Hello,
We have developed a BLDC driver around the DRV8306 IC to drive a BLDC motor. The datasheet of the motor is attached and the schematic of our PCB is attached.
The issue we are experiencing is that during no load testing, the…