Hi Luis,
Thanks for your reply.
1) Yes, t he non-inverting input is left floating, with the INA240 disconnected from the op-amp.
2) The output +1.26V is measured by an external meter.
INA240-SEP is replace to INA149-EP currently, and it is…
Part Number: INA240 Tool/software: Please provide a valid link to the "INA240-SEP Single-Event Latch-Up (SEL) Radiation Report" . It appears that the previous link is no longer valid (the datasheet has also been removed).
1. Yes, the status is "active".
2. There aren't that many space-rated devices. The INA240-SEP has different electrical characteristics.
3a. The part numbers are described in section 3 of the datasheet.
b. That depends for what you want to use it…
Hey Mathieu,
The current INA240A2 model shows that its linear output begins at around 45mV, which aligns with the 50mV Vout testing condition for gain error; however, Vout min at 0V Vin is around 29mV and this does not align with the 10mV specification…
Part Number: INA240 Hello,
In one of our designs, we has originally planned on using a rad-hard INA240-SEP current sense amplifer with 20V/V gain, but ended up purchasing the INA240A4PWR (200V/V gain) due to long lead time issues. Because of this, our…
Hello Astro,
They are not in the same process. So you cannot compare the two. Also we have other packaging the helps with this. Please see https://www.ti.com/product/INA240-SEP
Antonio,
Thanks for using E2E!
Unfortunately we have not done any radiation testing (SEE, SEL, etc.) to date on the TMCS110x family, nor do we have any reliability data for these devices in radiation based environments. Only parts designated as -SEP…
Part Number: LM193QML-SP Other Parts Discussed in Thread: INA901-SP , OPA4277 , , LM193
Hi teams,
My customer wants to use LM193QML-SP to detect current (INA901-SP/INA240-SEP) and voltage (OPA4277),
and he is wondering how to deal with the Vref…
Obinna,
Unfortunately, the only other enhanced device that we have is the INA240-SEP, which does not have the same radiation standards that the INA901 does. The INA901-SP is nearly complete and should look to re-release by the end of the third quarter…
Other Parts Discussed in Post: INA901-SP 作者:德州儀器 Kyle Stone
本文提及的產品: INA901-SP 、 INA240-SEP
目前已有幾家商用衛星業者大舉跨足太空領域,為這項過去多為政府出資的活動掀起一場革命。每年發射衛星數量之所以必須增加,主要是因為有些企業想在低軌道(low-Earth orbit)、中軌道(middle-Earth orbit)和地球同步軌道(geostationary equatorial orbit)…