Hello
It depends on what features and specs the customer is interested in.
I have attached a list of compatible devices that you may want to consider.
Thanks
Book1.xlsx
Other Parts Discussed in Thread: LM22675 , TINA-TI Hello,
I am trying to add the LM22675 spice model into LTspice, can some one help in how to go about this?
Thanks, MR
Other Parts Discussed in Thread: LM22675 I want to use two LM22675 Simple Switchers on my symmetrical +/-15V power supply. Setting up the +15V design is too easy -- use Webench.
However, Webench does not offer the LM22675 as a solution for the -15V supply…
Part Number: LM2675 Other Parts Discussed in Thread: LM22675 , , LM2594 Greetings,
My customer is looking for a drop in replacement for the LM2675M-ADJ/NOPB they are using. I saw that the LM22675 is P2P, however is it ok to use without soldering the thermal…
Other Parts Discussed in Thread: LM22675 Hello
I'm having some issues with feedback resistors when trying to get 9.0V out with a 12V input.
Webench suggests using Rfb1 = 430R and Rfb2 = 330R. However this only makes Vout around 2.3V with a 12V input…
Hi Lennart,
Proper connection of the EP is actually very important for this part, not just for heatsinking but also for optimal electrical functioning/protection. And with part failure its often times not just one thing but a summation of many parasitics…
Here's the design I've implemented -- www.stubbylatheusa.com/pdf/webench_design_3519623_8.pdf. This is the supply for a low volume commercial product. I'm not really an engineer but I've had a pretty good run of successes designing working boards…
Part Number: LM2674 Other Parts Discussed in Thread: LM2671 , LM22675 , LM22672 We have several designs using the LM2674MX-5.0 and this part seems very difficult to source at the moment. I am looking for an alternative part pin to pin compatible which could…
Other Parts Discussed in Thread: LM22675 , LM2937 Dear Sir,
I' m designing an electronic board for a device that will be mounted on trucks.
My idea is to use this components with the related components:
+24V 5V circuitry …