Part Number: LM3697 Hello:
Customer use TI‘s LM3697 for smart phone and the competitor is AW99703 from Awinic
The following diagram is the current schematic of AW99703
Among them, the pull-up resistance of SCL and SDA is 2.2K.
Please help confirm…
Part Number: LM3697 Hi,
Some questions for the LED current tolerance and would like to check with BU.
1. According to datasheet, the first line spec in captured below is around 10% tolerance and the 2nd line is +3.4% ~ -3.2%.
They are all in 20.2mA LED…
Part Number: LM3697 Other Parts Discussed in Thread: LP8867-Q1 Hi Sir,
My customer is asking about the minimum value for the PWM pulse width of LM3697, could you share the info with us?
Part Number: LM3697 Hi team,
At present, the registers configured by the software are as follows:
0x24 > 1 (enable control A)
0x10 > 0 (ch1/ch2/ch3 use control A) 0x19 > 7 (enable ch1/ch2/ch3 feedback)
However, we only use the channel of ch1…
Part Number: LM3697 Hi team,
Could you provide the DEVICE ID register of LM3697? My customer wants to read it for avoiding contrast.
Best Regards,
Peter
Part Number: LM3697 Other Parts Discussed in Thread: LP5562 , LP5813 Hi team,
My customer is looking for the alternative of AW2015, attachment is its datasheet. (Better P2P)
Can you help check this issue?
Awinic-AW2015FCR.pdf
Thanks!
Best regards
Lillian…
Hi Roy,
I'll close this thread due to inactivity and if you have more questions, please reply to it directly and it will open again.
Please help to click "Resolve" if the problem is solved.
BR
Patrick