Part Number: LM43602-Q1 Other Parts Discussed in Thread: LM63625-Q1 Dear TI,
Does LM43602-Q1 support asil b iso26262 or do we have similar device that can support asil b iso26262? Thanks.
Part Number: LM43602-Q1 I have a LM43602-Q1 converter that is converting 12V to 5V and running at 500kHz. We are seeing a large amount of EMI that appears to be coming specifically from the boost cap. Waveforms from each side of the cap shown below. If…
Part Number: LM43602-Q1 Hi,
I am looking into the datasheet of LM43602-Q1. Maximum rating of VIN is 42V under 'max duty cycle 0.01% of 10000 hours' note. What do the 'duty cycle' and '10000 hours' referred to? Thanks for your help!…
Part Number: LM43602-Q1 Other Parts Discussed in Thread: LM53602-Q1 , LM43602 , LM53603
Hello,
I'd like to ask some questions about LM43602-Q1.
At the input voltage of 6 to 6.5 V that will not rise further, will a LM43602-Q1 switch its switching mode…
Part Number: LM43602-Q1 Hello,
Would you let me know how the equality 19 and 20 in the datasheet shown below were derived?
Or make a brief explanation about what is compared to what in these inequalities?
One of my customers is making a lot of trouble…
Other Parts Discussed in Thread: LM43602-Q1 , LM43601-Q1 Hello,
The Voutp-p simulation result of LM43602-Q1, LM43601-Q1 on Webench was about 100mV~120mV. Is this result correct? I think that this is error in webench. If yes, could you please correct the Webench…
Part Number: LM63615-Q1 Other Parts Discussed in Thread: LM43602 , LM73605 , LMR33620 , LM60430 Hi,
I have an engineer with a project that is currently using 2x LM63615, but those are out of stock everywhere.
The requirement is for Vin =24V (spikes on dump…
Part Number: TPS3808-Q1 Other Parts Discussed in Thread: LM43602 , LM43602-Q1
Hi team.
My customer designed reset circuit as the below.
They added pull-up resistor(R2 : 4.7kohm) between SENSE to /MR.
If MCU does not control /MR(/MR input signal is High…
We do not have test conditions exactly match your request. But we do have something similar and can be used as a reference. On page 35 of the LM43602-Q1 datasheet www.ti.com/.../lm43602-q1.pdf , Figure 64 shows a relation shape of Theta JA and cooling…