Part Number: LM5033 Other Parts Discussed in Thread: LM5030 Hi team,
In our design, we are planning to replace LM5030 (Current mode PWM controller) with LM5033 (Voltage mode PWM controller)
What are the necessary changes we need to do, to use LM5033 in…
Part Number: LM5033 Will thermal protection work if IC is powered externally from 15 v supply with following options:
1. With V IN 15 V
2. With no V IN input
Part Number: LM5033 Hi,
I am curious about the internal frequency showed in datasheet of LM5033, when the Rt=26.7kohm, the variation of internal frequency is as big as plus minus 25kHz.
Even over the whole temp range it is quite big. Would you mind kindly…
Part Number: LM5033 Other Parts Discussed in Thread: TL431 , Design parameters:1、full-bridge circuit
2、Output Voltage:±190V
3、Output current:25A
During debugging, the no-load output voltage is normal. When the load…
Part Number: LM5033 Other Parts Discussed in Thread: LM358B My app involves two independent power supplies pulsed alternately ON and OFF (i.e. when one is ON the other is OFF). OFF state is generated by grounding SS. If I have an opamp follower driving…
Part Number: LM5033 Can we provide any reliability testing data for this part?
Things like the PCT Test (pressure cooker test), or the THB Test (Temperature Humidity Bias), etc?
If not, I know the datasheet has the max/min ratings over temperature, but…
Part Number: LM5033 Other Parts Discussed in Thread: LM5107 , LM5030 I have a customer using the LM5033/LM5107 in a similar implementation as shown in the Datasheet (Figure 11); only the system has 24V input and 12V output.
They have a test criteria that…
Part Number: LM5033 Dear e2e Support,
My customer is using 1x LM5033 to provide the bias voltages (+15V, -9V) to 6x IGBT drivers, for a brushless motor driver application.
He had some noise issue on his board and finally solved it by putting a 1nF capacitor…
Part Number: LM5033 Hi Team,
My customer evaluates it using the LM5033MM.
The external sync is working, but the duty is not close to 50%.
ON OFF Duty is 30% -70% operation, which is unstable operation which is 70% -30%.
If it is operated without a sync…