Part Number: LM5101A Hi all,
I am currently testing a MOSFET driver with the aim of the MOSFETS to be used in Cuk Converter for battery balancing applications.
I am feeding 2 synchronized 5kHz PWM signals from a ESP32 which are amplified before inputting…
Part Number: LM5100A Hi, we are now facing this issue.
In the part number LM5100A datasheet stated as below:
If the criteria that stated in the datasheet highlighted as below not meet, what is the impact and will it cause damage to the component with a…
Hey Nison,
Thank you for reaching out regarding the mechanical information for the UCC27212.
We have recently released a revision for this datasheet and during the release process the mechanical data was not properly added to the datasheet. We are aware…
Part Number: LM5101A Other Parts Discussed in Thread: INA240 Hi,
I attached a reliable design for ec-motor control with a 24 V supply.
Actually I exmaine wether this design is also working with a 48V power supply, an I found, that is no problem,
because…
Part Number: LM5101A Hello team,
Most gate driver products have peak current rating specifications (DC and pulse) in the Absolute Maximum Ratings table. However, this product does not specify the maximum peak current of the output terminal (HO-3 terminal…
Part Number: LM5101A Other Parts Discussed in Thread: LM5101 Hi TI Team,
I am facing LM5101A HS and GND short circuit issue. I need your support to resolve. I will share all data by mail. Kindly support by offline.
Regards,
Kubendran
Part Number: LM5101A Hi
in customer's system, LM5101A is used to drive hard switch full bridge MOSFETs
below is the waveform on HO-HS, -2.75V negative voltage can be seen.
customer want to know if LM5101A can support this -2.75V? is there any risk…
Part Number: LM5101A Dear Sir,
Could you confirm the operating temperature range of part number:
LM5101ASD-1/NOPB
Datasheet not mentioned any detail.
Thanks and Regards,
Nesh
Part Number: LM5101A Other Parts Discussed in Thread: LM5101 , Hello.
LM5101 finds problems in testing, and TI needs to help confirm.
When LM5101 is used, when the LM5101 5pin(HI) and 6pin(LI) level are low, the 3pin(HO) level output is high. The actual…
Part Number: LM5101A Other Parts Discussed in Thread: UCC27210 Hi, team,
My customer has one question about LM5101A, please help look into it and reply.
In LM5101A datasheet abs. maximum ratings table, LO output min is -0.3V. Is it a DC voltage value…