Part Number: LM5175EVM-HD Other Parts Discussed in Thread: LM5175 I want to limit the output current of the LM5175 integrated circuit. When it reaches 11A, the system should automatically shut down. How can I achieve this?
Part Number: LM5175EVM-HP Other Parts Discussed in Thread: LM5175 Hi
we need to boost 5v to 12V 12 AMP, whether this EVM support for 5V input
can I use this EVM for 5V input?
(The LM5175 is a synchronous 4-switch buck-boost controller capable of regulating…
Hello Karcel,
As we did not hear back from you, I expect the issue is solved and I will close this thread now. Please post below or start a new thread for further questions.
Best regards, Brigitte
Part Number: LM5175EVM Hi Expert
as below discussion, VIN=11.3V~11.7V, 12.4V~12.8V, 14.3V~15V the reason for the signal not consist that the value of Cslope.
LM5175EVM: gate driver signal not consist - Power management forum - Power management - TI E2E…
Hello Mona,
Thanks for the details in the other thread. Please let's discuss in the other thread and close this one for now. We are digging into the detail at the moment but will need some more days to get back to you.
Best regards, Brigitte
Part Number: LM5175-Q1 Other Parts Discussed in Thread: LM5175EVM , LM5175 Hi Experts,
We want to modify LM5175EVM to support min Vin 3.5V. How can we do that?
Regards,
Uchikoshi
Finally downloaded the LM5175EVM-HD design files. Modified the PCB from 6 layers to 4 and changed the mosfets, shunt and coil footprint. Released in production some samples. Lets see, will update results once will receive.
Part Number: LM5175EVM Other Parts Discussed in Thread: LM5175 Hi,
I use LM5175 for a reference design for 12~19Vin and 12Vout
But I got an issue for IC controller broken at switch on off test and short protection.
Is that I don't use 8.2V ZD at both SW…