Hi Rahul,
I apologize for the delay here. I have been able to test an unit in a temperature-controlled environment setup and can confirm that the device will default to the J2 gain (-5.166mV/C) when the Rsense pins are left open and no resistors are used…
Part Number: LM57 Hi all
My customer is looking for the package drawing / package dimensions for the LM57BISD-5/NOPB (package WSON – NGR 8)
This is not in the datasheet and also no dimensions for the document found at https://www.ti.com/support-packaging…
Part Number: LM57 We’re looking into using the LM57 as a temp sensor to switch off a load when the chip temp rises above -37C. We want to guarantee that the load is switched on from -55C to -37C.
Our low level functional temp range is -55C; this…
Part Number: LM57 If I want to measure ambient more accurately, should I remove the ground or any plane under LM57 to limit the heat picking up from the board?
Part Number: LM57 Other Parts Discussed in Thread: TMP300 , TMP107 Customer requested an automatic temperature trip point in each of their digital modules, to force a heating of the processor when the temperature is below a set point like −35°C for instance…
Part Number: LM57 Hi,
We are planning to use LM57 in one our application.
The application works from -55 deg C. LM57 will act as thermostatic switch in our application.
Tover threshold = -35 degC.
when temperature < -35 degC , Tover#(Open drain) will…
Part Number: LM57-Q1 Other Parts Discussed in Thread: LM57 Hi Team
If LM57 Rsense1 or Rsense2 short to GND. What temperature will be show or What will happened
Part Number: LM57
A customer is experiencing glitches on the output of the LM57. The device is applied into a noisy environment and it was verified there is noise reflected on Vsense 1 & 2. Do we have any input filtering guidelines? Furthermore, does…