Part Number: LMG1020EVM-006 Other Parts Discussed in Thread: TIDA-01573 , LMG1020 Hello TI engineers:
So far, I have tested The LMG1020EVM-006 with R5-R8 . But I had to test a real laser diode to see the drive capability of the EVM.
I saw the results of…
Part Number: LMG1020EVM-006
Hi,
According to EVM's D/S, "Switching frequency 0.1min ~ 50 MHz max", is it acceptable to use a one-shot pulse? If not, is there a recommended EVM?
Best regards,
Hiroshi
Part Number: LMG1020EVM-006 Other Parts Discussed in Thread: TIDA-01573 , LMG1020
I want to drive LD SPL TL90AT08 (IF = 40 A; tp = 100 ns; D = 0.01 %, Vop=11V) with an avalanche transistor. I need to produce trains of 100 nc square pulses with 1000 ns…
Part Number: LMG1020EVM-006 Hi Experts,
Good day. I am posting this inquiry on the customer's behalf.
Below is the full transcript of the customer's concern.
"We ordered the LMG1020EVM-006 evaluation board and I'm not getting anything on the…
Part Number: LMG1020EVM-006 Other Parts Discussed in Thread: LMG1020 Is there a recommended laser diode and configuration required to obtain 1-2ns pulses? Cause with normal Led(for testing purpose) after removing R5-R8 resistors I am only receiving continuous…
Part Number: LMG1020EVM-006
Hi team,
I have bought "LMG1020EVM-006" few days ago and tested it for a days.
And I found some overshoot (or undershoot?) problem in optical signal.
I attached laser diode (2.5GHz, 10mW) to eval board for make 1…
Part Number: LMG1020EVM-006 Hi Sir,
customer have question as follow.
the following reference design, if 2A need to increase the output current of 5A , is there any to modify it or suggest it?
Part Number: LMG1020EVM-006 I just received the LMG1020-EVM board. Despite comments in the online manual, the board comes pre-populated with four
4 ohm resistors in spots R5-R8. In the manual, the R5-R8 resistors are mentioned as not included with the…
Part Number: DAC39RF10EVM Other Parts Discussed in Thread: LMG1020EVM-006 , DAC39RF10 , DAC39RF12 , LMG1020 Hi,
Could I utilize the combination of LMG1020EVM-006 + DAC39RF10EVM to design something that can output minimum 300ps short pulse? the main reason…