Hi Paula, I use custom board.
root@am57xx-evm:~# dmesg [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 4.19.94-gbe5389fd85 (root@Pc) (gcc version 8.4.0 (Ubuntu/Linaro 8.4.0-1ubuntu1~18.04)) #1 SMP PREEMPT Tue Aug 11 13:11:26…
Part Number: CDCLVP111 Tool/software: Hi,
I would like to get your input on CDCLVP111 recommended termination bias voltage.
From Figure 11 of application report SLLA120 (Interfacing Between LVPECL, VML, CML, and LVDS Levels) and from literature in…
Thank you for the response. I have another question that is your datasheet reliable? because we have bought the X1243BIGABL based on the datasheet (SWRS188 –MAY 2017, page 4) that is attached, in which you mentioned the IC supports cascading but in 2018…
Hi, TI Expert
I also try to boot with the pre-built binaries as suggested one in this thread , while got the same result as above : "end Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b". The deatiled log info is below.
…
Part Number: TMDSLCDK6748
Hello all,
1)In Single-precision IIR filter (used in the VSELP vocoder) code present ,
for (i = 0; i < nr; i++)
sum = h2[0] * x[4+i]; why h2[0] is taken instead of h2[i] and i is added with 4?
2)
r1[nr+4] Delay element…
Hi,
OK, got it.
On the other hand, I remove DT node which related with lp8733. And i hanged on "Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b"
Could you help me to analyze this problem? Thanks
The whole log is below:…
Hi ,
We backported the ULPI driver from kernel 4.4 to kernel 3.14 , but we encounter the kernel panic ...
Please see the attach file and provide some advices.
Best,
Andy
Fullscreen
dmesg_0809_dwc3_probe.txt
Download
[ 0.000000…